2024-10-08 10:48 PM
[VERSION]: MCSDK.6.3.0
[TOOL]: ST Motor Pilot V1.2.9
[DETAILS]: BLDC motor, 12V, single pole pair.
I want to control the motor via a PWM signal. I am able to send pwm signal through onboard uart pins available from J7 RX/TX pins, into a new variable called P1. Now how do I assign the scaled value acquired from PWM to give to the onboard ADC pin available through TP4 ( variable pin on the onboard potentiometer) .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.