2024-09-02 6:34 AM
Hello there,
I am trying to generate 6 Step motor control firmware for some custom hardware based on the B-G431B-ESC1.
I would like to use the ESC PWM input feature, however the auto-generated code throws errors. This feature works fine in FOC mode, and I have tried to fix the errors by copying across the code generated in the FOC project and changing the TIMER configurations, but to no avail.
The problem is described in this post:
Error when generating code with MC Workbench 6.3.0 - STMicroelectronics Community
The responses there suggested this would be fixed in the 6.3.1 release. Is there any news on when this version will become available, or would it be possible to gain access to the beta?
Many thanks
2024-10-09 11:30 PM
Hello @SquirrelySquirrel99,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.