STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! MC SDK documentation for data packet structure?

Hi,I am trying to understand the protocol, especially how to interpret the data packets to have custom code for auto motor ramp-up.I see there are some documents under MC workbench -> About. However, I still cannot find the details about the data pac...

MC Observer + Cordic

I am trying to operate an 8-pole pair 48V PMSM motor withSTEVAL-CTM009V1IHM09M2Nucleo-G431RBSensorless with Observer + Cordic. I have run a motor profile with EVALSTDRIVE101. I have entered the parameters for the motor in MC Workbench 6.3.1. I have s...

ktim by Associate II
  • 2258 Views
  • 3 replies
  • 0 kudos

PWM highlight Timer

Hello, I am new in STM32Cube. I try some test with PWM timer 4. It  works. I see the signal on oscilloscope. But why is not in clock configuration  highlighted the timer clock and I can not also change the clock source.Best regards.  

Scipio_0-1728316741615.png Scipio_1-1728316770363.png
Scipio by Associate
  • 1006 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G4 - XCUBE-DPOW

Good day,we are currently integrating the XCUBE-Dpow library but are running into multiple issues due to the lack of code documentation of the library.- We are not using HTIM Channel-C but -D. After changing multiple entries in the template files of ...

JuculianD_0-1727782220410.png

Resolved! evspin32f0602s1 motor driving

Hello, I am very new for ST MCU,I have made may own evspin32f0602s1 board , after many trial and errors also after gone through documentation  ,I got  PWM output. but problem is that I  getting it at Reserved pins of MCU (TP1,TP2,TP3 in evolution boa...

KVijay32 by Associate II
  • 9281 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.