2019-07-02 3:26 AM
I am designing a data logger with STM32L4.
I want to transfer the data stored in STM32L4 to a Windows 10 PC by USB CDC.
USB full speed transfer is 12Mbps and transfer overhead at CDC overhead, so I think STM32L4 can be about 4 to 6Mbps.
Who is know transfer speed can be?
2019-07-02 3:48 AM
I think your estimations are accurate; I remember approaching about 800KB/s speeds using STM32F407's USB FS CDC, which is a bit higher than your estimated 6Mbps.
2019-07-02 9:03 PM
thank you for your comment.
2019-07-04 12:19 AM
hi After Forever and everyone
I want your suggestion.
I connected a laptop (Windows 10) and STM32L4 (60 MHz) with a USB cable.
90 Kbytes of data were sent from the PC to the STM32L4 internal RAM using the USB FS CDC.
The transfer time was 7 seconds.
It is about 103 kbps.
I think it's slow, is it like this?
STM32F7 has faster clock than STM32L4 CPU.
Do you think that the clock speed is fast and the communication speed is fast?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.