2019-07-03 12:20 AM
2019-07-03 12:54 AM
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0646a/Ciheijba.html
Therefore alignment depends on specific MCU, but it definitely isn't as high as 0x8000 bytes.
2019-07-03 1:59 AM
according to link, it seems should work as long as the app address's least 7 bits are 0.
2019-07-03 2:53 AM
It is usually a function of the vector table size in a given implementation. Take the last vector and round to the next binary multiple, on most STM32 likely 512 byte boundaries.
2019-07-03 8:02 PM
thank for your reply. for stm32f303, my app scatter file is
LR_IROM1 0x0800C000 0x00032000 { ; load region size_region
ER_IROM1 0x0800C000 0x00032000 { ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
.ANY (+XO)
}
RW_IRAM1 0x20000000 0x0000C000 { ; RW data
.ANY (+RW +ZI)
}
RW_IRAM2 0x10000000 UNINIT 0x00002000 {
mode_keys.o (+RW)
exception_mem.o (+RW)
}
}
my bootloader jump process is
typedef void (*pFunction)(void);
pFunction Jump = (pFunction) (*(uint32_t*)(FLASH_ONCHIP_APP + 4));
SCB->VTOR = FLASH_ONCHIP_APP;
__set_MSP(*(uint32_t*)FLASH_ONCHIP_APP);
Jump();
Why it does not work?
2019-07-03 8:11 PM
>>Why it does not work?
I don't know, use the debugger, step into the code, across the transition and understand what is actually happening.
Is some downstream code changing SCB->VTOR? Are you calling from interrupt/callback context?
Do you turn off other interrupt sources? SysTick, etc
do you have a Hard Fault Handler, or Error Handler that output useful information?
2019-07-04 1:34 AM
fixed. I forgot set VECT_TAB_OFFSET
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.