2024-09-17 5:30 AM - last edited on 2024-09-23 1:52 PM by Pavel A.
I'm trying to get USBX Device MSC to work in Standalone mode (without RTOS). I loosely followed @B.Montanari 's example in https://community.st.com/t5/stm32-mcus/how-to-implement-usbx-in-standalone-mode/ta-p/614435, and also referred to a CubeMX example for Device MSC which does use an RTOS (STM32Cube_FW_U5_V1.6.0\Projects\STM32U575I-EV\Applications\USBX\Ux_Device_MSC). I'm running this on an STM32U5 dev kit.
There are no errors, Windows recognizes the USB MSC device, and a drive shows up. But something isn't working quite right, since Windows tells me to insert a disk, won't format the volume, and doesn't seem to recognize its size.
I'm not quite sure yet where things are going wrong, but I thought I'd see if this configuration is expected to work or if I'm overlooking any other examples before digging further...
Solved! Go to Solution.
2024-09-23 1:09 PM - edited 2024-09-23 2:16 PM
This was apparently caused by a bug in the USBX source. Once I fixed it, things seem to be working.
It looks like _ux_device_class_storage_disk_wait just passes the return value of ux_slave_class_storage_media_read (and other similar functions) directly to _ux_device_class_storage_task_disk. Here this return value is compared against UX_STATE_NEXT to check for success.
However, comparing some additional samples and other places in the code, ux_slave_class_storage_media_read is expected to return UX_SUCCESS if successful.
BTW, while debugging through the code I also found a couple of bugs in _ux_utility_debug_log (as-is it won't even compile with the UX_ENABLE_DEBUG_LOG switch).
This makes me wonder whether Standalone mode and other non-mainstream features are getting much use or test time.
2024-09-17 5:42 AM
Hello @PRuss ,
Try to increase the heap size or configure the USB library to use static allocation as recommended in this FAQ: USB device not recognized.
2024-09-20 5:33 AM
Thanks for the reply. I did increase both the heap and stack significantly, but I'm still having the same issue.
2024-09-23 1:09 PM - edited 2024-09-23 2:16 PM
This was apparently caused by a bug in the USBX source. Once I fixed it, things seem to be working.
It looks like _ux_device_class_storage_disk_wait just passes the return value of ux_slave_class_storage_media_read (and other similar functions) directly to _ux_device_class_storage_task_disk. Here this return value is compared against UX_STATE_NEXT to check for success.
However, comparing some additional samples and other places in the code, ux_slave_class_storage_media_read is expected to return UX_SUCCESS if successful.
BTW, while debugging through the code I also found a couple of bugs in _ux_utility_debug_log (as-is it won't even compile with the UX_ENABLE_DEBUG_LOG switch).
This makes me wonder whether Standalone mode and other non-mainstream features are getting much use or test time.
2025-01-16 8:43 AM
Hello @PRuss
I'm also trying to get USBX MSC to work in standalone mode for one of my projects. However, I can't get it to work. In my main loop, I call the ux_device_stack_tasks_run function, which allows me to detect my device when I plug it into Windows.
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
ux_device_stack_tasks_run();
//_ux_device_class_storage_tasks_run(storage);
}
/* USER CODE END 3 */UINT MX_USBX_Device_Init(VOID)
{
UINT ret = UX_SUCCESS;
UCHAR *device_framework_high_speed;
UCHAR *device_framework_full_speed;
ULONG device_framework_hs_length;
ULONG device_framework_fs_length;
ULONG string_framework_length;
ULONG language_id_framework_length;
UCHAR *string_framework;
UCHAR *language_id_framework;
UCHAR *pointer;
/* USER CODE BEGIN MX_USBX_Device_Init0 */
/* USER CODE END MX_USBX_Device_Init0 */
pointer = ux_device_byte_pool_buffer;
/* Initialize USBX Memory */
if (ux_system_initialize(pointer, USBX_DEVICE_MEMORY_STACK_SIZE, UX_NULL, 0) != UX_SUCCESS)
{
/* USER CODE BEGIN USBX_SYSTEM_INITIALIZE_ERROR */
return UX_ERROR;
/* USER CODE END USBX_SYSTEM_INITIALIZE_ERROR */
}
/* Get Device Framework High Speed and get the length */
device_framework_high_speed = USBD_Get_Device_Framework_Speed(USBD_HIGH_SPEED,
&device_framework_hs_length);
/* Get Device Framework Full Speed and get the length */
device_framework_full_speed = USBD_Get_Device_Framework_Speed(USBD_FULL_SPEED,
&device_framework_fs_length);
/* Get String Framework and get the length */
string_framework = USBD_Get_String_Framework(&string_framework_length);
/* Get Language Id Framework and get the length */
language_id_framework = USBD_Get_Language_Id_Framework(&language_id_framework_length);
/* Install the device portion of USBX */
if (ux_device_stack_initialize(device_framework_high_speed,
device_framework_hs_length,
device_framework_full_speed,
device_framework_fs_length,
string_framework,
string_framework_length,
language_id_framework,
language_id_framework_length,
UX_NULL) != UX_SUCCESS)
{
/* USER CODE BEGIN USBX_DEVICE_INITIALIZE_ERROR */
return UX_ERROR;
/* USER CODE END USBX_DEVICE_INITIALIZE_ERROR */
}
/* Initialize the storage class parameters for the device */
storage_parameter.ux_slave_class_storage_instance_activate = USBD_STORAGE_Activate;
storage_parameter.ux_slave_class_storage_instance_deactivate = USBD_STORAGE_Deactivate;
/* Store the number of LUN in this device storage instance */
storage_parameter.ux_slave_class_storage_parameter_number_lun = STORAGE_NUMBER_LUN;
/* Initialize the storage class parameters for reading/writing to the Flash Disk */
storage_parameter.ux_slave_class_storage_parameter_lun[0].
ux_slave_class_storage_media_last_lba = USBD_STORAGE_GetMediaLastLba();
storage_parameter.ux_slave_class_storage_parameter_lun[0].
ux_slave_class_storage_media_block_length = USBD_STORAGE_GetMediaBlocklength();
storage_parameter.ux_slave_class_storage_parameter_lun[0].
ux_slave_class_storage_media_type = 0;
storage_parameter.ux_slave_class_storage_parameter_lun[0].
ux_slave_class_storage_media_removable_flag = STORAGE_REMOVABLE_FLAG;
storage_parameter.ux_slave_class_storage_parameter_lun[0].
ux_slave_class_storage_media_read_only_flag = STORAGE_READ_ONLY;
storage_parameter.ux_slave_class_storage_parameter_lun[0].
ux_slave_class_storage_media_read = USBD_STORAGE_Read;
storage_parameter.ux_slave_class_storage_parameter_lun[0].
ux_slave_class_storage_media_write = USBD_STORAGE_Write;
storage_parameter.ux_slave_class_storage_parameter_lun[0].
ux_slave_class_storage_media_flush = USBD_STORAGE_Flush;
storage_parameter.ux_slave_class_storage_parameter_lun[0].
ux_slave_class_storage_media_status = USBD_STORAGE_Status;
storage_parameter.ux_slave_class_storage_parameter_lun[0].
ux_slave_class_storage_media_notification = USBD_STORAGE_Notification;
/* USER CODE BEGIN STORAGE_PARAMETER */
/* USER CODE END STORAGE_PARAMETER */
/* Get storage configuration number */
storage_configuration_number = USBD_Get_Configuration_Number(CLASS_TYPE_MSC, 0);
/* Find storage interface number */
storage_interface_number = USBD_Get_Interface_Number(CLASS_TYPE_MSC, 0);
/* Initialize the device storage class */
if (ux_device_stack_class_register(_ux_system_slave_class_storage_name,
ux_device_class_storage_entry,
storage_configuration_number,
storage_interface_number,
&storage_parameter) != UX_SUCCESS)
{
/* USER CODE BEGIN USBX_DEVICE_STORAGE_REGISTER_ERROR */
return UX_ERROR;
/* USER CODE END USBX_DEVICE_STORAGE_REGISTER_ERROR */
}
/* USER CODE BEGIN MX_USBX_Device_Init1 */
/* Initialize the USB Peripheral */
MX_USB_OTG_FS_PCD_Init();
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_FS, 0x80);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_FS, 0, USBD_MAX_EP0_SIZE / 4);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_FS, 1, USBD_MSC_EPIN_FS_MPS / 2);
/* Link the USB drivers with the USBX DCD and check if it return error */
if(ux_dcd_stm32_initialize((ULONG)USB_OTG_FS, (ULONG)&hpcd_USB_OTG_FS) != UX_SUCCESS)
{
Error_Handler();
}
if(ux_dcd_stm32_initialize((ULONG)USB_OTG_FS, (ULONG)&hpcd_USB_OTG_FS) != UX_SUCCESS)
{
Error_Handler();
}
/* Start the PCD Peripheral */
HAL_PCD_Start(&hpcd_USB_OTG_FS);
/* USER CODE END MX_USBX_Device_Init1 */
return ret;
}However, I never get as far as the USBD_STORAGE_Read or USBD_STORAGE_Write functions. As far as I can see, this is because I don't call the _ux_device_class_storage_tasks_run function.
If this is the problem, how can I retrieve the storage class instance?
Thanks for your help
2025-06-03 8:53 AM
Hey @PRuss
What firmware change did you implement to fix the _ux_device_storage_disk_wait bug?
Thanks!
Peter
2025-07-05 7:49 PM
Thank you so much! I modified the code based on your idea, and now the USBX MSC standalone mode works for me.
These are the changes that made it work
static inline UINT _ux_device_class_storage_disk_wait(UX_SLAVE_CLASS_STORAGE *storage)
{
UINT status = UX_SUCCESS;
switch (storage -> ux_device_class_storage_cmd)
{
case UX_SLAVE_CLASS_STORAGE_SCSI_READ16:
case UX_SLAVE_CLASS_STORAGE_SCSI_READ32:
status = (storage -> ux_slave_class_storage_lun[storage -> ux_slave_class_storage_cbw_lun].
ux_slave_class_storage_media_read(storage,
storage -> ux_slave_class_storage_cbw_lun,
storage -> ux_device_class_storage_buffer[
storage -> ux_device_class_storage_buffer_disk],
storage -> ux_device_class_storage_disk_n_lb,
storage -> ux_device_class_storage_cmd_lba,
&storage -> ux_device_class_storage_media_status));
return (status == UX_SUCCESS) ? UX_STATE_NEXT : UX_STATE_ERROR;
case UX_SLAVE_CLASS_STORAGE_SCSI_WRITE16:
case UX_SLAVE_CLASS_STORAGE_SCSI_WRITE32:
status= ( storage -> ux_slave_class_storage_lun[storage -> ux_slave_class_storage_cbw_lun].
ux_slave_class_storage_media_write(storage,
storage -> ux_slave_class_storage_cbw_lun,
storage -> ux_device_class_storage_buffer[
storage -> ux_device_class_storage_buffer_disk],
storage -> ux_device_class_storage_disk_n_lb,
storage -> ux_device_class_storage_cmd_lba,
&storage -> ux_device_class_storage_media_status));
return (status == UX_SUCCESS) ? UX_STATE_NEXT : UX_STATE_ERROR;
case UX_SLAVE_CLASS_STORAGE_SCSI_SYNCHRONIZE_CACHE:
status = ( storage -> ux_slave_class_storage_lun[storage -> ux_slave_class_storage_cbw_lun].
ux_slave_class_storage_media_flush(storage,
storage -> ux_slave_class_storage_cbw_lun,
storage -> ux_device_class_storage_disk_n_lb,
storage -> ux_device_class_storage_cmd_lba,
&storage -> ux_device_class_storage_media_status));
return (status == UX_SUCCESS) ? UX_STATE_NEXT : UX_STATE_ERROR;
case UX_SLAVE_CLASS_STORAGE_SCSI_VERIFY: /* No nothing for now. */
default:
break;
}
return(UX_STATE_NEXT);
}2025-08-13 4:30 PM
Hi, Could you share the github link of the working project ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.