2025-11-19 6:16 AM
Please refer to this thread that, for some reason, @FBL accepted as an answer (it is not) https://community.st.com/t5/stm32-mcus-embedded-software/usbx-audio-class-frame-done-callback-not-called/td-p/855262
I'm seeing that when I try to start an audio flux from my PC to the USB Audio driver, I'm seeing the error handler being called with the following stack:
status = _ux_device_stack_transfer_request(transfer, max_packet_size, max_packet_size); triggers the error as the status is 38 (what does it mean?). Inside the function, I've found
status = dcd -> ux_slave_dcd_function(dcd, UX_DCD_TRANSFER_REQUEST, transfer_request);which is the one that returns 38.
In ux_api.h, the only value I was able to find that matches the return value was
#define UX_TRANSFER_BUS_RESET 0x26From here, I'm stuck as the ux_slave_dcd_function is defined as
typedef struct UX_SLAVE_DCD_STRUCT
{
UINT ux_slave_dcd_status;
UINT ux_slave_dcd_controller_type;
UINT ux_slave_dcd_otg_capabilities;
UINT ux_slave_dcd_irq;
ULONG ux_slave_dcd_io;
ULONG ux_slave_dcd_device_address;
UINT (*ux_slave_dcd_function) (struct UX_SLAVE_DCD_STRUCT *,UINT, VOID *);
void *ux_slave_dcd_controller_hardware;
} UX_SLAVE_DCD;
Solved! Go to Solution.
2025-11-28 12:30 AM
The issue has been traced back to a bug in the USBX library
2025-11-19 7:00 AM
Hi @nico23
I've answered you in the original post! It would be better to address different issues in different posts to avoid misinterpretation.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-19 7:02 AM
Please, feel free to delete this post and keep the original one.
The issue is always one, the frame done callback not being called.
2025-11-28 12:30 AM
The issue has been traced back to a bug in the USBX library
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.