STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Generate a single pulse of 12ns with stm32u5

Hi there.I’m trying to generate a 12 ns pulse for a time-of-flight (ToF) application.I’m using an STM32U5 microcontroller, and I’d like to know whether one of the general-purpose timers (TIM2/TIM3/TIM4/TIM5) can produce a pulse that narrow. With a 16...

USB_Microphone: not audio output

Hi everyone. I am relatively new to working with STM32 devices, and I am currently attempting to design a USB microphone with an analog input using the Nucleo-L476RG development board in combination with the X-NUCLEO-CCA02M2 USB audio expansion board...

USBX MSC SD card + FILEX SD card problem

Hi, i'm trying to make a firmware that can read an SD card with filex but that can also connect that SD card to USBX MSC device (no simultaney). i'm able to do the two functionality in two separate firmware, but the problem is to merge. for now is su...

ABasi.2 by Senior
  • 1591 Views
  • 9 replies
  • 0 kudos

Resolved! GPIO output not working

Hi, I’m working on an STM32G491 MCU and facing an issue with GPIO PB9.In my project, I initialize PB9 as a digital output and try to set it HIGH, but the pin always stays LOW on the board.However, if I configure PB9 as input and toggle the pin extern...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.