2019-05-04 5:36 PM
I create Custom hid and send 2 PC report using
while(1){
USBD_CUSTOM_HID_SendReport(&hUsbDeviceFS, dataToSend, 4);
}
And... Device is frozen. Why? I am going inside HAL->USBD_CUSTOM_HID_SendReport... I see code
hhid->state = CUSTOM_HID_BUSY;
so USBD_CUSTOM_HID_SendReport function makes devise busy but no one can make device unbusy. Is it ok?
Solved! Go to Solution.
2019-05-05 10:14 AM
The endpoint is marked "unbusy" when the host sends IN request and the controller spews the queued data on the wire. If this does not occur -either the host does not read, or something is wrong with setup of USB controller & device.
-- pa
2019-05-04 5:59 PM
Please check your device descriptor and endpoint descriptor to check whether it works correct or not.
Normally it depends on the size or endpoint buffer setting wrong.
2019-05-05 10:14 AM
The endpoint is marked "unbusy" when the host sends IN request and the controller spews the queued data on the wire. If this does not occur -either the host does not read, or something is wrong with setup of USB controller & device.
-- pa
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.