2024-08-19 7:43 PM
I am using the NUCLEO-G474RE along with the X-NUCLEO-SRC1M1 board to create a USB-C power delivery source. I am also using the "SRC1M1_Source" example project in the x-cube-tcpp software download.
I am attempting to provide a 20V, 5000mA source to a USB-C power delivery sink. After I connect the nucleo board to the STM32CubeMonitor-UCPD, I am able to add the 20V, 5000mA PDO and send it to the target.
I plug the sink device into my SRC1M1 board (trace data attached)
I see the sink requests the 20V, 5000mA profile, however the trace data shows USBPD_CAD_STATE_DETACH_SRC soon after the profile is accepted by my source. The connection and negotiation then start again and continue in an infinite loop.
I am supplying the SRC1M1 board with an external power supply set to 5V. I had assumed that the source would not indicate SRC_READY until I manually adjusted the supply voltage to 20V, however it just disconnects.
What is the proper way to use the SRC1M1 source board to establish a 20V contract with a sink device?
Solved! Go to Solution.
2024-08-26 7:54 AM
Hi @captat
Thanks for sharing your case.
PSready should be sent only once 20V is ready.
About the unexpected detach (1017107), it may be due to SINK event (like a Vbus protection). Could you check Vbus voltage ? (You could use trace system to display VBUS level like explained here.)
Have a look at the G0 demonstration on the G0 Evaluation board in github. Are you using functions similar to USBPD_PWR_IF_SetProfile and BSP_USBPD_PWR_VBUSSetVoltage_Fixed ?
I put here a trace of the G0 evaluation messages (Port 1 = SRC, On the G0 Evaluation board we have a DCDC that need to be controlled with a PWM) :
We have a request of PDO3 (15V), and we can observe between PE_SRC_TRANSITION_SUPPLY and PE_SRC_TRANSITION_SUPPLY_EXIT some delay to adjust VBUS, and then we can send the PS RDY.
CAD 361617 1 USBPD_CAD_STATE_EMC 0
CAD 361625 1 USBPD_CAD_STATE_SWITCH_TO_SNK 1
CAD 361627 1 USBPD_CAD_STATE_DETACHED 2
CAD 361701 1 USBPD_CAD_STATE_ATTACHED_WAIT 3
CAD 361791 1 USBPD_CAD_STATE_ATTEMC 5
NOTIF 361791 1 USBSTACK_START 6
DEBUG 361791 1 USBIF host start 7
EVENT 361791 1 EVENT_ATTEMC 8
DEBUG 361791 1 EN_VBUS 9
DEBUG 361791 1 CC:2 VCONN:1 10
DEBUG 361791 1 VCONN ON 11
DEBUG 361791 1 VBUS ON 12
DEBUG 361792 1 duty_c=176:cal=:0 13
DEBUG 361810 1 ca5V:433 14
PE 361810 1 PE_SRC_STARTUP 15
NOTIF 361810 1 POWER_STATE_CHANGE 16
PE 361810 1 PE_CABLE_VDM_DISCOVERY_REQUEST 17
OUT 361812 1 SOP1 s:006 PD3 H:0x108F (id:0, DR:UFP, PR:SNK) VENDOR_DEFINED
VDM:SVDM_DISCOVER_IDENTITY INIT DATA:01A800FF
18
OUT 361813 1 SOP1 s:006 PD3 H:0x108F (id:0, DR:UFP, PR:SNK) VENDOR_DEFINED
VDM:SVDM_DISCOVER_IDENTITY INIT DATA:01A800FF
19
OUT 361815 1 SOP1 s:006 PD3 H:0x108F (id:0, DR:UFP, PR:SNK) VENDOR_DEFINED
VDM:SVDM_DISCOVER_IDENTITY INIT DATA:01A800FF
20
PE 361817 1 PE_SRC_SEND_CAPABILITIES 21
OUT 361825 1 SOP PD3 s:022 H:0x51A1 (id:0, DR:DFP, PR:SRC) SRC_CAPABILITIES DATA: 2C9101232CD102002CB104003C32DCC03C3240C1
Option: UNCHUNK DRD DRP
[1] Fixed : 5V - 3A
[2] Fixed : 9V - 3A
[3] Fixed : 15V - 3A
[4] Programmable : [5V - 11V] - 3A
[5] Programmable : [5V - 16V] - 3A
30
IN 361827 1 SOP s:002 H:0x0041 (id:0, DR:UFP, PR:SNK) GOODCRC 33
NOTIF 361827 1 SRCCAP_SENT 34
PE 361827 1 PE_SRC_WAIT_REQUEST 35
IN 361829 1 SOP PD3 REQUEST s:006 H:0x1082 (id:0, DR:UFP, PR:SNK) DATA: 96588231
ObjectPosition:3
GiveBack:0
CapabilityMismatch:0
USBCommunicationCapable:0
NoUSBSuspend:1
UnchunkedExtendedMessagesSupported:1
MaximumOperatingCurrent:1500mA
OperatingCurrent:1500mA 39
OUT 361829 1 SOP s:002 H:0x0161 (id:0, DR:DFP, PR:SRC) GOODCRC 40
PE 361830 1 PE_SRC_NEGOTIATE_CAPABILITY 43
OUT 361832 1 SOP PD3 ACCEPT s:002 H:0x03A3 (id:1, DR:DFP, PR:SRC) 44
IN 361833 1 SOP s:002 H:0x0241 (id:1, DR:UFP, PR:SNK) GOODCRC 47
PE 361833 1 PE_SRC_TRANSITION_SUPPLY 48
NOTIF 361863 1 POWER_STATE_CHANGE 52
DEBUG 361863 1 duty_c=432:cal=:0 53
DEBUG 361927 1 ca15V:2746 56
DEBUG 361932 1 V:15043(count=1) 57
PE 361932 1 PE_SRC_TRANSITION_SUPPLY_EXIT 58
OUT 361934 1 SOP PD3 PS_RDY s:002 H:0x05A6 (id:2, DR:DFP, PR:SRC) 59
IN 361935 1 SOP s:002 H:0x0441 (id:2, DR:UFP, PR:SNK) GOODCRC 62
NOTIF 361935 1 POWER_STATE_CHANGE 63
NOTIF 361935 1 POWER_EXPLICIT_CONTRACT 64
You can also have a look at STEVAL-2STPD01 with associated software.
It’s a USB Type-C Power Delivery dual port adapter based on the STPD01 programmable buck converter with a STM32G071RE on NUCLEO + 2x TCPP02-M18 + 2x STPD01.
Input DC voltage of the buck is 24V and each USB-C port can deliver 20V – 3A independently. Ant the voltage control is done thanks to an I2C bus.
2024-08-26 7:54 AM
Hi @captat
Thanks for sharing your case.
PSready should be sent only once 20V is ready.
About the unexpected detach (1017107), it may be due to SINK event (like a Vbus protection). Could you check Vbus voltage ? (You could use trace system to display VBUS level like explained here.)
Have a look at the G0 demonstration on the G0 Evaluation board in github. Are you using functions similar to USBPD_PWR_IF_SetProfile and BSP_USBPD_PWR_VBUSSetVoltage_Fixed ?
I put here a trace of the G0 evaluation messages (Port 1 = SRC, On the G0 Evaluation board we have a DCDC that need to be controlled with a PWM) :
We have a request of PDO3 (15V), and we can observe between PE_SRC_TRANSITION_SUPPLY and PE_SRC_TRANSITION_SUPPLY_EXIT some delay to adjust VBUS, and then we can send the PS RDY.
CAD 361617 1 USBPD_CAD_STATE_EMC 0
CAD 361625 1 USBPD_CAD_STATE_SWITCH_TO_SNK 1
CAD 361627 1 USBPD_CAD_STATE_DETACHED 2
CAD 361701 1 USBPD_CAD_STATE_ATTACHED_WAIT 3
CAD 361791 1 USBPD_CAD_STATE_ATTEMC 5
NOTIF 361791 1 USBSTACK_START 6
DEBUG 361791 1 USBIF host start 7
EVENT 361791 1 EVENT_ATTEMC 8
DEBUG 361791 1 EN_VBUS 9
DEBUG 361791 1 CC:2 VCONN:1 10
DEBUG 361791 1 VCONN ON 11
DEBUG 361791 1 VBUS ON 12
DEBUG 361792 1 duty_c=176:cal=:0 13
DEBUG 361810 1 ca5V:433 14
PE 361810 1 PE_SRC_STARTUP 15
NOTIF 361810 1 POWER_STATE_CHANGE 16
PE 361810 1 PE_CABLE_VDM_DISCOVERY_REQUEST 17
OUT 361812 1 SOP1 s:006 PD3 H:0x108F (id:0, DR:UFP, PR:SNK) VENDOR_DEFINED
VDM:SVDM_DISCOVER_IDENTITY INIT DATA:01A800FF
18
OUT 361813 1 SOP1 s:006 PD3 H:0x108F (id:0, DR:UFP, PR:SNK) VENDOR_DEFINED
VDM:SVDM_DISCOVER_IDENTITY INIT DATA:01A800FF
19
OUT 361815 1 SOP1 s:006 PD3 H:0x108F (id:0, DR:UFP, PR:SNK) VENDOR_DEFINED
VDM:SVDM_DISCOVER_IDENTITY INIT DATA:01A800FF
20
PE 361817 1 PE_SRC_SEND_CAPABILITIES 21
OUT 361825 1 SOP PD3 s:022 H:0x51A1 (id:0, DR:DFP, PR:SRC) SRC_CAPABILITIES DATA: 2C9101232CD102002CB104003C32DCC03C3240C1
Option: UNCHUNK DRD DRP
[1] Fixed : 5V - 3A
[2] Fixed : 9V - 3A
[3] Fixed : 15V - 3A
[4] Programmable : [5V - 11V] - 3A
[5] Programmable : [5V - 16V] - 3A
30
IN 361827 1 SOP s:002 H:0x0041 (id:0, DR:UFP, PR:SNK) GOODCRC 33
NOTIF 361827 1 SRCCAP_SENT 34
PE 361827 1 PE_SRC_WAIT_REQUEST 35
IN 361829 1 SOP PD3 REQUEST s:006 H:0x1082 (id:0, DR:UFP, PR:SNK) DATA: 96588231
ObjectPosition:3
GiveBack:0
CapabilityMismatch:0
USBCommunicationCapable:0
NoUSBSuspend:1
UnchunkedExtendedMessagesSupported:1
MaximumOperatingCurrent:1500mA
OperatingCurrent:1500mA 39
OUT 361829 1 SOP s:002 H:0x0161 (id:0, DR:DFP, PR:SRC) GOODCRC 40
PE 361830 1 PE_SRC_NEGOTIATE_CAPABILITY 43
OUT 361832 1 SOP PD3 ACCEPT s:002 H:0x03A3 (id:1, DR:DFP, PR:SRC) 44
IN 361833 1 SOP s:002 H:0x0241 (id:1, DR:UFP, PR:SNK) GOODCRC 47
PE 361833 1 PE_SRC_TRANSITION_SUPPLY 48
NOTIF 361863 1 POWER_STATE_CHANGE 52
DEBUG 361863 1 duty_c=432:cal=:0 53
DEBUG 361927 1 ca15V:2746 56
DEBUG 361932 1 V:15043(count=1) 57
PE 361932 1 PE_SRC_TRANSITION_SUPPLY_EXIT 58
OUT 361934 1 SOP PD3 PS_RDY s:002 H:0x05A6 (id:2, DR:DFP, PR:SRC) 59
IN 361935 1 SOP s:002 H:0x0441 (id:2, DR:UFP, PR:SNK) GOODCRC 62
NOTIF 361935 1 POWER_STATE_CHANGE 63
NOTIF 361935 1 POWER_EXPLICIT_CONTRACT 64
You can also have a look at STEVAL-2STPD01 with associated software.
It’s a USB Type-C Power Delivery dual port adapter based on the STPD01 programmable buck converter with a STM32G071RE on NUCLEO + 2x TCPP02-M18 + 2x STPD01.
Input DC voltage of the buck is 24V and each USB-C port can deliver 20V – 3A independently. Ant the voltage control is done thanks to an I2C bus.
2024-08-27 7:31 PM
Thanks for the pointers. Turns out, the USBPD_PWR_IF_SetProfile function I was using was hard coded to use the first PDO profile, not the 20V profile the sink was requesting. Using the code in the github link you provided as an example, I was able to get my setup working. Additionally, I needed to switch the source voltage much more quickly. Seems like the voltage needed to be switched within several hundred milliseconds or a hard reset would occur.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.