2026-02-24 10:25 PM
I am able to receive UDP unicast packets on the Nucleo-h563ZI using the netconn API, however I cannot receive broadcast UDP packets (global or subnet). I have attached my lwiopts.h for reference along with the relevant discovery service code below. Note that netif->flags has NETIF_FLAG_BROADCAST set in addition to NETIF_FLAG_ETHARP. I was unable to find any broadcast related settings in the IOC file for the ETH peripheral nor related HAL_ETH_xyz calls. I did try enabling broadcast in the MACFilter, but this had no effect.
#define NET_TASK_DISCO_PORT (5555)
#define NET_TASK_DISCO_REQUEST "SCPI_DISCOVERY"
#define NET_TASK_DISCO_RESPONSE "SCPI_DEVICE"
#define NET_TASK_DISCO_RESP_LENGTH (64)
//
// @brief Discovery application
// @return none
//
static void disco(void *pArgument)
{
char response[NET_TASK_DISCO_RESP_LENGTH];
uint16_t length;
void *pBuffer;
void *pSend;
struct netbuf *prBuffer;
struct netbuf *prSend;
trNet *prNet = (trNet*)pArgument;
// Validate argument[s]
ASSERT(NULL != prNet);
// Create connection and bind to port
if (NULL == (prNet->rDisco.prConnection = netconn_new(NETCONN_UDP)))
{
LOGERROR(eErrorOutOfResources);
return;
}
netconn_bind(prNet->rDisco.prConnection, IP_ADDR_ANY, NET_TASK_DISCO_PORT);
// Forever loop
for(;;)
{
// Receive request
if (ERR_OK == netconn_recv(prNet->rDisco.prConnection, &prBuffer))
{
// Get receive buffer
netbuf_data(prBuffer, &pBuffer, &length);
LOG(eLogLevelDebug, "%s", pBuffer);
// Check request
if (0 == strncmp(pBuffer, NET_TASK_DISCO_REQUEST, length))
{
// Get send buffer
if (NULL != (prSend = netbuf_new()))
{
// Build response
snprintf(response, sizeof(response) - 1,
"%s;IDN=%s;IP=%s;PORT=%u", NET_TASK_DISCO_RESPONSE,
"SPPTS-101", "192.168.0.10", NET_TASK_DISCO_PORT);
LOG(eLogLevelDebug, "%s", response);
// Allocate and copy buffer
pSend = netbuf_alloc(prSend, strlen(response));
memcpy(pSend, response, strlen(response));
// Send response
netconn_sendto(prNet->rDisco.prConnection, prSend,
netbuf_fromaddr(prBuffer), netbuf_fromport(prBuffer));
// Return send buffer
netbuf_delete(prSend);
}
}
// Return buffer
netbuf_delete(prBuffer);
}
}
}Here is the successful response when sending a unicast packet:
bob@xyz:~$ echo -n "SCPI_DISCOVERY" | nc -u 192.168.50.123 5555
SCPI_DEVICE;IDN=SPPTS-101;IP=192.168.0.10;PORT=5555
Relevent settings in lwipopts.h
#define IP_SOF_BROADCAST 1
#define IP_SOF_BROADCAST_RECV 1
#define LWIP_BROADCAST_PING 1
2026-02-25 1:55 AM
Your ethernet driver is not boradcast enabled.
Check eth setting or share your code and we can show how to enable.
2026-02-25 9:34 AM
2026-03-02 3:49 PM - edited 2026-03-02 3:50 PM
Just checking in as I have not received a reply after uploading the ethernetif code.
2026-03-03 1:18 AM
What's the content of ETH_MACPFR register?
JW
2026-03-07 10:23 AM
2026-03-08 1:46 PM
I don't think you'd need the promiscuous mode to be enabled.
What I was thinking was, that the broadcasts are disabled by ETH_MACPFR.DBF being set - but as you've shown that's not the case here.
At this point you should have the 'H5 board isolated from any network traffic, so that you can transmit to it in a controlled way, and observe (e.g. in debugger) at the ETH level, what packets are received and which are rejected/filtered.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.