2022-06-08 11:36 AM
I decided to try to use the __HAL_ADC_ENABLE_IT() macro. UM2319 page 95/2202 Rev 2
It says the first argument is the ADC handle.
ADC_HandleTypeDef hadc1; is the handle.
This macro wants the ADC handle pointer which is &hadc1 not hadc1.
Looks like the other macros in this section may have the same documentation issue.
2022-06-09 12:36 AM
Hi @KiptonM ,
Thank you for reporting this.
But I do not think this is an issue because the ADC Handle is a parameter of type #Struct of #Struct.
And looking at this macro description, only the #Struct Instance of the ADC Handle is used.
#define __HAL_ADC_ENABLE_IT(__HANDLE__, __INTERRUPT__) \
(((__HANDLE__)->Instance->IER) |= (__INTERRUPT__))
With all that to use this macro, you need to pass the pointer of ADC Handle otherwise you will have a compiling C error.
Best Regards,
A.MVE
2022-06-10 9:14 AM
Exactly. You need the pointer. to the handle, not the handle. That is what the issue is.
The handle is hadc1. It is a structure. You can directly use it with hadc1.***
The pointer to the handle is &hadc1. (& means take the address of the item, a.k.a. a pointer.)
This you have to use as hadc1->*** there is a difference.
You need to use the pointer to the handle (&hadc1). The handle (hadc1) will not work.
What would you have called it if you needed to use hadc1 (not &hadc1) and the macro was written
#define __HAL_ADC_ENABLE_IT(__HANDLE__, __INTERRUPT__) \
(((__HANDLE__).Instance->IER) |= (__INTERRUPT__))
You would have said use the "handle"
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.