STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Not able to create semaphore in lwIP stack

Hi ,I am working on STM32L072 controller with RTOS which communicates with LAN9250 ethernet IC over SPI . i have integrated the lwIP stack in ,my project externally (v2.1.3). I am using netconn api's for data tx and rx. While creating net connection ...

0693W00000Hnet7QAB.png
BChav.1 by Associate III
  • 1161 Views
  • 0 replies
  • 0 kudos

USB HID Device response with a STALL

Hello everyone,I have trouble while implementing USB HID on a STM32F373.I use the "custom Human Interface device class" and implemented all like in the video from ST Link. I also tested my device with the HID Terminal from the video (the Programm jus...

0693W00000HneolQAB.png
DSchu.6 by Associate
  • 1029 Views
  • 0 replies
  • 0 kudos

Resolved! FATFS not working when if FreeRTOS is enabled

Hello, I've a STM32 NUCLEO board (STM32F446RETx) with an SD card board connected to it.Im using:STM32CubeIDE Version: 1.7.0 Build: 10852_20210715_0634 (UTC)STMicroelectronics STM32CubeMX 6.3.0.202107141111 com.st.stm32cube.common.mxSTM32CubeF4 Firmwa...

JBren.3 by Associate
  • 1953 Views
  • 2 replies
  • 1 kudos

Resolved! Some help with the USB on the STM32F446VET .

Hi , I'm writing here to ask community some help with the F446VET chip. I tried the Cube Ide and CubeMX to perform all the settings.What have been done so far :In the USB_DEVICE--> Class for FS IP is set to "Communication Device Class(Virtual Port C...

MBolo.1 by Associate III
  • 2275 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.