2021-10-12 6:52 PM
Hi
I'm trying to read the output from BARCODE reader (ES4650) using USB-HOST using CDC type.
On connecting the USB cable I'm getting SOF interrupts (although I disable the Signal SOF on CUBE). On pointing the barcode reader to a barcode I'm getting some USB interrupt causes (USB_OTG_GINTSTS_RXFLVL and USB_OTG_GINTSTS_HCINT - both for IN and OUT).
On getting those interrupts I'm looking in the USB data buffer and see no data.
The CDC Class is as follow:
USBH_ClassTypeDef CDC_Class =
{
"CDC",
USB_CDC_CLASS,
USBH_CDC_InterfaceInit,
USBH_CDC_InterfaceDeInit,
USBH_CDC_ClassRequest,
USBH_CDC_Process,
USBH_CDC_SOFProcess,
NULL,
};
The code never reach those functions.
I was accepting using other drivers functions as USBH_CDC_Receive or USBH_CDC_ReceiveCallback but as you can see, the CUBE defines others.
What do I do wrong ?
Thanks
2021-10-12 10:43 PM
Maybe the device is not CDC ACM compliant. Check the descriptors it sends (maybe when connected to PC, e.g. using lsusb if you are using Linux).
JW
2021-10-14 3:11 AM
Hi JW
The device support both USB-HOST virtual com-port and USB-HOST HID (keyboard).
I tested the HID mode and it works like a charm, so I don't have to test the CDC anymore - thanks anyway.
Ofer
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.