2023-01-06 4:14 PM
/* Check if software trigger enabled */
if ((hdac->Instance->CR & (DAC_CR_TEN1 | DAC_CR_TSEL1)) == DAC_CR_TEN1)I think the if check is wrong - we should check if TEN and TSEL are set, but now we check for TSEL=111 and TEN=0
2023-01-08 5:19 PM
Currently it checks for exactly the opposite: TEN=1 and TSEL1=0. Supposedly it is the line 590 of the HAL driver code. The line 599 is also wrong. And the correct solution seems to be like the line 611. Also the block of code at the line 611 could be merged with the block at line 590 if...
Edited by moderating team to adhere to community guidelines
2023-01-13 10:07 AM
Yup. Apparently noone ever used HAL for SW trigger (it makes sense when you want to use TRIANGLE or NOISE generation without HW trigger).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.