STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to enter UART bootloader on STM32G030K6T6?

I'm trying to activate the UART bootloader after receiving input (from either a button press or from parsing a command from UART interrupt). I see from the G030x programming manual that to do so, I must set bits of the FLASH_OPTR register as nBOOT1 =...

GWork by Associate
  • 3615 Views
  • 3 replies
  • 0 kudos

FreeRTOS implementation with X-Cube-BLE2

I'm trying to implement a BLE task in my FreeRTOS application with the X-Nucleo-BNRG2A1 shield. I completed the BLE application (X-Cube-BLE2 package) without FreeRTOS and it has been working fine. For implementing the FreeRTOS, I have been looking in...

I try to implement UART DMA reception in circular buffer with reception with idle in STM32F429 Discovery with MCU Package for STM32F4 in Rev 1.27.0 . IDLE event is not called when number of recived char rise DMA_TC.

What i expect is that my interrupt callback (HAL_UARTEx_RxEventCallback) will be called with those event :DMA_Half_Transfert Complete -> OKDMA_Transfert_Complete -> OKIDLE_Event -> OKAll interrupt work individually but...1) Receive buffer is emptyI s...

Ethernet issue (STM32F7BIT)

Posted on October 12, 2017 at 14:40Hello .,I am working on STM32 MCU in our custom board, In this I am facing some issues related to Ethernet interface. I manage to generate Ethernet code using STM cube MX,(Using in RMII), The code is working but no...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.