2025-02-18 12:18 AM - last edited on 2025-04-14 3:40 AM by mƎALLEm
Dear ST Community,
I am working on an Ethernet TCP/IP project using the Nucleo-F746ZG development board with the LWIP stack, without any RTOS. I have based my implementation on the tcp_echoclient example driver file. The project builds successfully, and the application runs in debug mode, but it does not work in release mode.
I have compared the map files for both release and debug modes but found no significant differences.
Additionally, I am facing issues with MPU configuration while using the LWIP stack. Specifically, I need clarification on:
Project Details:
I would appreciate any guidance on these issues. Thank you in advance!
2025-06-11 12:44 AM
Hello @aKM_,
It appears that is a timing or synchronization issue.
Please take a look at this post: Solved: Basic UDP Echo server works in debug, but not run ... - STMicroelectronics Community
With Regards,
2025-07-07 9:33 AM
Hello @aKM_ ,
Please try the solution below:
During the initialization process, the ETH MAC must be configured with the correct Ethernet link speed and duplex mode after the auto-negotiation process is completed, which can take up to few seconds (see the API HAL_ETH_SetMACConfig).
Add a call to the API Ethernet_Link_Periodic_Handle in your main loop.
This API will periodically polls the PHY status and updates the MAC configurations if any changes occur to the Ethernet link.
An example can be retrieved in "STM32F769I_EVAL\Applications\LwIP\LwIP_HTTP_Server_Raw" application in STM32CubeF7 v1.17.0 package.
Note: There is no need to add an additional HAL_delay().
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.