cancel
Showing results for 
Search instead for 
Did you mean: 

STR32F411RE Board for VL53L4CD (GUI)

chosuwan
Associate

Hello

I have a few questions

Situation Summary:

  • Development board: STM32F411RE

  • Sensor: VL53L4CD TOF sensor

  • Previous successful case: On the STM32F401RE board, setting the BOOT0 pin to 1 → uploading the BIN file via STM32CubeProgrammer → sensor operation verified successfully via GUI.

Current issue (STM32F411RE board):

  • Setting BOOT0 the same way as on the F401 → STM32CubeProgrammer connection is lost.

  • Using the adjacent JP1 pin (instead of the originally used one) → BIN file download succeeds.

  • Running the GUI program → board and COM port not detected.

  • Running "FLASH FW" in the GUI → port is detected, but the sensor shows a "not detected" message.

Note: Both the F401RE and F411RE boards use the JP1 pin next to the board’s power pins as the BOOT pin.

Question: What is the recommended method to make the sensor work properly with the GUI on the STM32F411RE board?

 

I would appreciate any guidance you could provide on this issue.

Please find my email address below.

thanks 

 

email : whtndhks@it-m.co.kr 

2 REPLIES 2
chosuwan
Associate

Problem solved!!

Hello @chosuwan 

Could you please share the solution. This could be helpful for other users who might encounter the same issue.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.