2025-10-09 11:44 AM
Hello superhero MCU enthusiasts,
I'm playing with the STM32N6570-DK and have created a simple project with an FSBL that initializes the MCU and boots the Appl. Once booted, the Appl flashes a "Hello World" LED.
Both can be loaded to external flash using the STM32CubeProgrammer.
Now, I'm trying to map external PSRAM (XSPI1 -> 0x90000000) inside the FSBL, but it fails.
To do that, I change a line in a file in the FSBL, stm32_extmem_conf.h, line 35 of (PSRAM disabled):
#define EXTMEM_DRIVER_PSRAM 0Now I try to enable and map the external PSRAM by setting the definition to 1:
#define EXTMEM_DRIVER_PSRAM 1However, it doesn't succeed.
When debugging I see we land into a HardFault.
The FSBL generates a HardFault when executing SAL_XSPI_EnableMapMode, because the function HAL_XSPI_MemoryMapped fails.
I can't find the cause.
Anyone?
I posted a project here with a short Readme.md:
https://github.com/AngryCarrot61/STM32N6570-DK_004
Note: to see FSBL and Appl working one has to set EXTMEM_DRIVER_PSRAM to 0.
However the goal is to get PSRAM mapped (XSPI1 at 0x90000000).
Flashing:
the debug directories for FSBL and Appl contain a batch file: '0_SigningTool.bat'.
After compiling, run the batch files to sign the binaries.
Using STM32CubeProgrammer we select EL 'MX66UW1G45G_STM32N6570-DK'.
FSBL will be loaded at 0x70000000, and Appl at 0x70100000.
Enjoy!
Any help is much apreciated regarding the part to map the PSRAM!
Cheers!
Solved! Go to Solution.
2025-10-10 7:15 AM - edited 2025-10-17 8:08 AM
Thank you very much, I forgot to add the PSRAM into the MPU.
However, the initialization still failes, so I wouldn't be able to access it anyway.
My new STM32N6 MPU configuration:
static void MPU_Config(void)
{
/*
* XSPI2 0x70000000 128MB FLASH (1-Gbit Octo-SPI)
* XSPI1 0x90000000 32MB PSRAM (256-Mbit Hexadeca-SPI)
*/
MPU_Region_InitTypeDef default_config = {0};
MPU_Attributes_InitTypeDef attr_config = {0};
uint32_t primask_bit = __get_PRIMASK();
__disable_irq();
/* disable the MPU */
HAL_MPU_Disable();
/* create an attribute configuration for the MPU */
attr_config.Attributes = INNER_OUTER(MPU_WRITE_BACK | MPU_NON_TRANSIENT | MPU_RW_ALLOCATE);
attr_config.Number = MPU_ATTRIBUTES_NUMBER0;
HAL_MPU_ConfigMemoryAttributes(&attr_config);
/* Create a region associated with memory address 0x70000000 */
/*Normal memory type, code execution allowed */
default_config.Number = MPU_REGION_NUMBER0;
default_config.Enable = MPU_REGION_ENABLE;
default_config.BaseAddress = XSPI2_BASE; /* FLASH 128MB 0x70000000 */
default_config.LimitAddress = XSPI2_BASE + 0x08000000-1;
default_config.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
default_config.AccessPermission = MPU_REGION_ALL_RO;
default_config.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
default_config.AttributesIndex = MPU_ATTRIBUTES_NUMBER0;
HAL_MPU_ConfigRegion(&default_config);
/* Ensure the FSBL enables MPU access for the PSRAM region before mapping it: */
default_config.Number = MPU_REGION_NUMBER1;
default_config.Enable = MPU_REGION_ENABLE;
default_config.BaseAddress = XSPI1_BASE; /* PSRAM 32MB 0x90000000 */
default_config.LimitAddress = XSPI1_BASE + 0x02000000-1;
default_config.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
default_config.AccessPermission = MPU_REGION_ALL_RW;
default_config.IsShareable = MPU_ACCESS_INNER_SHAREABLE | MPU_ACCESS_OUTER_SHAREABLE;
default_config.AttributesIndex = MPU_ATTRIBUTES_NUMBER0;
HAL_MPU_ConfigRegion(&default_config);
/* enable the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
/* Exit critical section to lock the system and avoid any issue around MPU mechanisme */
__set_PRIMASK(primask_bit);
}I still hope to find the problem soon. I'm looking into my PSRAM initialization.
Thanks for helping!
UPDATE: I got access to the external PSRAM working from the FSBL.
I added HAL_PWREx_EnableVddIO* lines.
void HAL_MspInit(void)
{
HAL_PWREx_EnableVddIO2();
HAL_PWREx_EnableVddIO3();
HAL_PWREx_EnableVddIO4();
HAL_PWREx_EnableVddIO5();
}After the PSRAM test, FSBL launches the application (Appl), which blinks the LEDs.
I updated the repository on github:
https://github.com/AngryCarrot61/STM32N6570-DK_004
Enjoy!
2025-10-10 7:15 AM - edited 2025-10-17 8:08 AM
Thank you very much, I forgot to add the PSRAM into the MPU.
However, the initialization still failes, so I wouldn't be able to access it anyway.
My new STM32N6 MPU configuration:
static void MPU_Config(void)
{
/*
* XSPI2 0x70000000 128MB FLASH (1-Gbit Octo-SPI)
* XSPI1 0x90000000 32MB PSRAM (256-Mbit Hexadeca-SPI)
*/
MPU_Region_InitTypeDef default_config = {0};
MPU_Attributes_InitTypeDef attr_config = {0};
uint32_t primask_bit = __get_PRIMASK();
__disable_irq();
/* disable the MPU */
HAL_MPU_Disable();
/* create an attribute configuration for the MPU */
attr_config.Attributes = INNER_OUTER(MPU_WRITE_BACK | MPU_NON_TRANSIENT | MPU_RW_ALLOCATE);
attr_config.Number = MPU_ATTRIBUTES_NUMBER0;
HAL_MPU_ConfigMemoryAttributes(&attr_config);
/* Create a region associated with memory address 0x70000000 */
/*Normal memory type, code execution allowed */
default_config.Number = MPU_REGION_NUMBER0;
default_config.Enable = MPU_REGION_ENABLE;
default_config.BaseAddress = XSPI2_BASE; /* FLASH 128MB 0x70000000 */
default_config.LimitAddress = XSPI2_BASE + 0x08000000-1;
default_config.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
default_config.AccessPermission = MPU_REGION_ALL_RO;
default_config.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
default_config.AttributesIndex = MPU_ATTRIBUTES_NUMBER0;
HAL_MPU_ConfigRegion(&default_config);
/* Ensure the FSBL enables MPU access for the PSRAM region before mapping it: */
default_config.Number = MPU_REGION_NUMBER1;
default_config.Enable = MPU_REGION_ENABLE;
default_config.BaseAddress = XSPI1_BASE; /* PSRAM 32MB 0x90000000 */
default_config.LimitAddress = XSPI1_BASE + 0x02000000-1;
default_config.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
default_config.AccessPermission = MPU_REGION_ALL_RW;
default_config.IsShareable = MPU_ACCESS_INNER_SHAREABLE | MPU_ACCESS_OUTER_SHAREABLE;
default_config.AttributesIndex = MPU_ATTRIBUTES_NUMBER0;
HAL_MPU_ConfigRegion(&default_config);
/* enable the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
/* Exit critical section to lock the system and avoid any issue around MPU mechanisme */
__set_PRIMASK(primask_bit);
}I still hope to find the problem soon. I'm looking into my PSRAM initialization.
Thanks for helping!
UPDATE: I got access to the external PSRAM working from the FSBL.
I added HAL_PWREx_EnableVddIO* lines.
void HAL_MspInit(void)
{
HAL_PWREx_EnableVddIO2();
HAL_PWREx_EnableVddIO3();
HAL_PWREx_EnableVddIO4();
HAL_PWREx_EnableVddIO5();
}After the PSRAM test, FSBL launches the application (Appl), which blinks the LEDs.
I updated the repository on github:
https://github.com/AngryCarrot61/STM32N6570-DK_004
Enjoy!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.