2017-07-14 2:59 AM
Hi everyone,
I'm working with an STM32L476VGT microcontroller and I'm trying to use USB_OTG_FS in Host_Only mode for reading and writing on an USB Drive.
I also have a STM32L476 Discovery board but cannot find any example using usb otg, fatfs and FreeRTOS. The system in standalone mode (without FreeRTOS) works flawlessly, but now I need task scheduling so having a RTOS is mandatory.I'm currently using CubeMX to generate code for both Discovery board and our custom board as well. The problem is that I cannot manage to make things work for (apparently) two different reasons.Since there's no example code for using USB Host library AND FreeRTOS in STM32Cube_FW_L4_V1.8.0 I started from STM32Cube USB host library User manual (UM1720) and some exaple code for STM32F4.On the Discovery Board the system detects when the drive is plugged and fires the HOST_USER_CONNECTION event and the drive is correctly mounted because f_mount() function returns FR_OK and the HOST_USER_CLASS_ACTIVE event follows as expected, the problem is that at this point f_open() function gets stuck in a while loop (usbh_msc.c line 726).In function USBH_MSC_Read() there is this while loop:while (USBH_MSC_RdWrProcess(phost, lun) == USBH_BUSY)
{ if(((phost->Timer - timeout) > (10000 * length)) || (phost->device.is_connected == 0)) { MSC_Handle->state = MSC_IDLE; return USBH_FAIL; }}but the condition never breaks because USBH_MSC_RdWrProcess() always returns USBH_BUSY (its switch-case statement verifies a parameter that always remains the same - MSC_INIT).
When I'm not using FreeRTOS, after few iterations, this parameter changes and the process works well.On our custom board there's a slightly different problem: the system detects when the drive is plugged, fires the HOST_USER_CONNECTION event, f_mount() returns FR_OK but the HOST_USER_CLASS_ACTIVE event never fires.
Is there anyone who have already had some similar issue and can point me to a possible solution?
#stm32l4 #usb #fatfs #freertos #usb_otg_fs2018-08-09 7:47 PM
Sorry, bumping old zombie unanswered questions off my feed
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.