2023-11-15 9:06 AM
Hello,
I am using a sTM32L430 with a JTAG access through ST LINK V2 and STM32CubeIDE.
This project was created with STM32CubeMx and mainly contains a while(1) loop toggling a led.
After a power the program starts correctly (led toggles and current consumption is around 2mA)
After a reset the program does not start and the current consumption is around 16mA.
I checked the reset signal state with an oscilloscope and the waveform is correct.
Do you have any idea?
Best regards
Mich
2023-11-15 11:22 AM
Starting a program from the IDE "run" button is different than by hardware reset or power-on. The IDE will force the PC to the "Reset_Handler" address in the elf file (comes from the startup_stm32Lxxxxxx.s file) - ignoring the PC value in the vector table. I don't recall off hand what it does with the stack pointer. Hardware reset or power-on will use the vector table entries for SP and PC.
So you may have some issues with the vector table. See if you have USER_VECT_TAB_ADDRESS defined to non-zero in system_stm32l4xx.c.
Other than that, use the debugger to set breakpoints in main() and in the assembly startup code then press the reset button and see what the code does.
2023-11-15 11:07 PM
It seems that it is an hardware issue with this hand soldered prototype.
I soldered a 2nd PCBA and there is not such issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.