2025-08-14 1:40 AM
So I want to use a capture compare to measure an input frequency 0.1Hz to 100kHz. Peripheral clock is set to 32MHz to cover full range and maximise speed of calculations. At lower frequency I have to count the number of times the over capture call-back is called, to put into the calculation. However there are a few frequencies where the over capture and edge detection IRQs have a beating effect, I have delt with this on other processors by ensuring the order IRQs are delt with but it doesn't seem to be working here.
Sometimes the last over capture is called first, other times in is not, leading to a large jump in my calculated result. As anyone any experience with this issue on the STM32 TIM peripherals?
/******************************************************************************
Function : Calculate_Frequency
Return : Frequency post calculation as a float
*****************************************************************************/
#define TIMCLOCK 32000000.00 //System clock value post PLL
#define PRESCALAR 1
unsigned int Pending_Result;
unsigned int Frequency_Counter_Overflow;
unsigned int IC_Val1_OFC;
unsigned int IC_Val2_OFC;
unsigned int Overflow_Difference;
unsigned int Last_Overflow_Count;
unsigned int IC_Val1;
unsigned int IC_Val2;
unsigned int Difference;
unsigned int IC_Val1_Array[8];
unsigned int IC_Val2_Array[8];
unsigned int Difference_Array[8];
unsigned int frequency_Array[8];
unsigned int Sum_Array[8];
unsigned int Overflow_Difference_Array[8];
unsigned int IC_Val1_OFC_Array[8];
unsigned int IC_Val2_OFC_Array[8];
unsigned int x;
unsigned int Sum_Used;
float frequency;
//This table removes the need for a multiplication, speeding up the capture to output time.
unsigned long Overflow_Lookup[256] = {
0, 65535, 131070, 196605, 262140, 327675, 393210, 458745, 524280, 589815, 655350,
720885, 786420, 851955, 917490, 983025, 1048560, 1114095, 1179630, 1245165, 1310700,
1376235, 1441770, 1507305, 1572840, 1638375, 1703910, 1769445, 1834980, 1900515, 1966050,
2031585, 2097120, 2162655, 2228190, 2293725, 2359260, 2424795, 2490330, 2555865, 2621400,
2686935, 2752470, 2818005, 2883540, 2949075, 3014610, 3080145, 3145680, 3211215, 3276750,
3342285, 3407820, 3473355, 3538890, 3604425, 3669960, 3735495, 3801030, 3866565, 3932100,
3997635, 4063170, 4128705, 4194240, 4259775, 4325310, 4390845, 4456380, 4521915, 4587450,
4652985, 4718520, 4784055, 4849590, 4915125, 4980660, 5046195, 5111730, 5177265, 5242800,
5308335, 5373870, 5439405, 5504940, 5570475, 5636010, 5701545, 5767080, 5832615, 5898150,
5963685, 6029220, 6094755, 6160290, 6225825, 6291360, 6356895, 6422430, 6487965, 6553500,
6619035, 6684570, 6750105, 6815640, 6881175, 6946710, 7012245, 7077780, 7143315, 7208850,
7274385, 7339920, 7405455, 7470990, 7536525, 7602060, 7667595, 7733130, 7798665, 7864200,
7929735, 7995270, 8060805, 8126340, 8191875, 8257410, 8322945, 8388480, 8454015, 8519550,
8585085, 8650620, 8716155, 8781690, 8847225, 8912760, 8978295, 9043830, 9109365, 9174900,
9240435, 9305970, 9371505, 9437040, 9502575, 9568110, 9633645, 9699180, 9764715, 9830250,
9895785, 9961320, 10026855, 10092390, 10157925, 10223460, 10288995, 10354530, 10420065,
10485600, 10551135, 10616670, 10682205, 10747740, 10813275, 10878810, 10944345, 11009880,
11075415, 11140950, 11206485, 11272020, 11337555, 11403090, 11468625, 11534160, 11599695,
11665230, 11730765, 11796300, 11861835, 11927370, 11992905, 12058440, 12123975, 12189510,
12255045, 12320580, 12386115, 12451650, 12517185, 12582720, 12648255, 12713790, 12779325,
12844860, 12910395, 12975930, 13041465, 13107000, 13172535, 13238070, 13303605, 13369140,
13434675, 13500210, 13565745, 13631280, 13696815, 13762350, 13827885, 13893420, 13958955,
14024490, 14090025, 14155560, 14221095, 14286630, 14352165, 14417700, 14483235, 14548770,
14614305, 14679840, 14745375, 14810910, 14876445, 14941980, 15007515, 15073050, 15138585,
15204120, 15269655, 15335190, 15400725, 15466260, 15531795, 15597330, 15662865, 15728400,
15793935, 15859470, 15925005, 15990540, 16056075, 16121610, 16187145, 16252680, 16318215,
16383750, 16449285, 16514820, 16580355, 16645890, 16711425};
float Calculate_Frequency (void)
{
if (Pending_Result == 1)
{
Overflow_Difference = (IC_Val2_OFC - IC_Val1_OFC); //work out how many periods have passed between edges
if (Overflow_Difference > 255) //it's a very slow frequency so we can work it out
{
if (IC_Val2 > IC_Val1) //no interim period to deal with
{
Difference = (Overflow_Difference * 0xFFFF) + (IC_Val2 - IC_Val1); //(total passed periods * full period count) + (second edge time - first edge time)
}
else if (IC_Val1 > IC_Val2) //interim period to deal with
{
Difference = (((Overflow_Difference) * 0xFFFF) - IC_Val1) + IC_Val2; //((total passed periods * full period count) - first edge time[interim]) + second edge time
}
}
else
{
if (IC_Val2 > IC_Val1) //no interim period to deal with
{
Difference = Overflow_Lookup[Overflow_Difference] + (IC_Val2 - IC_Val1); //(total passed periods * full period count) + (second edge time - first edge time)
Sum_Used = 1;
}
else if (IC_Val1 > IC_Val2) //interim period to deal with
{
Difference = (Overflow_Lookup[Overflow_Difference] - IC_Val1) + IC_Val2; //((total passed periods * full period count) - first edge time[interim]) + second edge time
Sum_Used = 2;
}
}
Frequency_Counter_Overflow = 0; //reset the period counter
__HAL_TIM_SET_COUNTER(&htim2, 0); // reset the counter
TIM2->SR &= ~TIM_SR_UIF; //clear the global IRQ flag, before re-enabling the IRQs
TIM2->SR = ~(TIM_SR_CC1OF | TIM_SR_TIF); // Clear the bitwise flags
__HAL_TIM_ENABLE_IT(&htim2, TIM_IT_CC1); //restart IRQ now calculations are complete
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_3, GPIO_PIN_SET);
frequency = TIMCLOCK/Difference;
Last_Overflow_Count = Overflow_Difference;
Pending_Result = 0; //clear the flag that a result is awaiting processing
//Bug trap code ----------------------------------------------------------------
IC_Val1_Array[x] = IC_Val1;
IC_Val2_Array[x] = IC_Val2;
Difference_Array[x] = Difference;
frequency_Array[x] = frequency;
Sum_Array[x] = Sum_Used;
Overflow_Difference_Array[x] = Overflow_Difference;
IC_Val1_OFC_Array[x] = IC_Val1_OFC;
IC_Val2_OFC_Array[x] = IC_Val2_OFC;
x++;
if (x>7)
{
x=0;
}
//Bug trap code end -------------------------------------------------------------
return (frequency);
}
else
{
if (Frequency_Counter_Overflow >= (Last_Overflow_Count + 250))
{
return(200000); //dummy value to show no calculation as been done, but enough time as passed that there is no valid signal
}
else
{
return(300000); //dummy value to show no calculation as been done
}
}
}
/******************************************************************************
ISR : Input Capture Callback
*****************************************************************************/
unsigned int Is_First_Captured;
unsigned int Miss_Intrim_Edge;
extern unsigned int Both_Edges;
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
{
if (Pending_Result == 0) //there is not already a result awaiting processing
{
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1)
{
if (Is_First_Captured==0) // if the first edge is not captured
{
IC_Val1_OFC = Frequency_Counter_Overflow; //record the period in which this edge occurred
IC_Val1 = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1); // read the first value
Is_First_Captured = 1; // set the first captured as true
}
else if ((Both_Edges == 1) && (Miss_Intrim_Edge == 0)) //miss the alternate edge, in all edges mode
{
Miss_Intrim_Edge = 1;
}
else if ((Both_Edges == 0) || (Miss_Intrim_Edge == 1)) // If the first edge is captured, now we will capture the second edge
{
IC_Val2_OFC = Frequency_Counter_Overflow; //record the period in which this edge occurred
IC_Val2 = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1); // read second value
Is_First_Captured = 0; // set it back to false
Miss_Intrim_Edge = 0; // set it back to false
Pending_Result = 1; //set flag that a result calculation is required
__HAL_TIM_DISABLE_IT(htim, TIM_IT_CC1); //stop IRQ to maximise calculation time
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_3, GPIO_PIN_RESET);
}
}
}
}
/******************************************************************************
ISR : Input Capture overflow
*****************************************************************************/
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
Frequency_Counter_Overflow ++; //a full timer period as passed, increment the period counter
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_2);
}
Solved! Go to Solution.
2025-08-14 2:37 AM
If your timer frequency is 32 MHz, using a 32-bit timer is sufficient to capture 0.1 Hz without overflow.
You can do it with a 16-bit timer but you'll run into race conditions if not done right.
2025-08-14 1:33 AM - edited 2025-08-14 1:42 AM
Sorry posted in the wrong place see
STM32L010C6 TIM2 IRQ Priority, Over capture Vs edg... - STMicroelectronics Community
2025-08-14 2:37 AM
If your timer frequency is 32 MHz, using a 32-bit timer is sufficient to capture 0.1 Hz without overflow.
You can do it with a 16-bit timer but you'll run into race conditions if not done right.
2025-08-14 3:04 AM
Thank you TDK, unfortunately the L0 series part only has 16 bit timers.
It is the race condition that is causing my issue, I have had this on other uC in the past but making sure the over capture flag in tested first normally fixes the issue, but not this time.
2025-08-14 3:05 AM
Hello,
If there is no timer instance supporting a 32 bit counter on your STM32L0 MCU, you can still chain 2 timers to increase the frequency range of your frequency measure and avoid to have to deal with capture overflows. To do so you can refer to the section 16.3.3 of the reference manual (RM0377). For instance, if TIM2 is configured in external clock mode 1, TIM3 TRGO can be used to feed the TIM2 counter through ITR2 interconnect.
2025-08-14 4:29 AM
Thank you Francois, I will take a look and give this a try.
2025-08-15 1:28 AM
Hello Francois, I have tried to implement this to no avail and then realised
RM0377 - STM32L0x1
I need
RM0451 - STM32L0x0
Looking at table 77, it suggests that timers can only be paired in certain ways, is my understanding correct?
I have my hardware input on T2 and was hoping to use T21 or T22 as the high order counter, due to already having hardware tracked for T2.
2025-08-15 1:52 AM - edited 2025-08-15 2:03 AM
It's nontrivial to use a couple of 16-bit timers to achieve 32-bit effective counting with maintaining granularity to the LSB. You would need to capture in both timers simultaneously, which means either to have the input signal brought to two pins in parallel, or have the capture signal traced through TRGO/TRGI from one timer to other and have a very good grasp at running the two timers simultaneously (one of them internally prescaled) and also characterize the undocumented delays of TRGO/TRGI.
Most guidelines would use one timer as a prescaler (master) to the other (slave) and then perform the capture at the slave; but that's effectively just the same as what you can achieve with using the "native" prescaler within one single timer.
JW
PS Just a technicality, you are not dealing with overcapture here, but with timer overflows.
Overcapture would mean that there are at least two captures before you succeed to handle any of them.
JW
2025-08-17 11:46 PM
Hello,
your understanding is correct. ITR0(TS=000) pairs TIM2/TIM21, ITR1(TS=001) pairs TIM2/TIM22, ...Actually, the programing of the TS bitfield selects the active input of a mux internally connected to a number of other timer instances trigger output.
As mentioned above there is another option where you can use the master timer as a prescaler of the master timer to 'slow down' the counting so that you can measure low frequencies.
Francois
2025-08-18 4:17 AM - edited 2025-08-18 4:21 AM
Thanks again for the help.
I looked at the master timer and pre-scaler however to avoid an overflow at 0.25Hz I would need to run at 16kHz (4 secs / 65536 = 61uS), so this is not an option as it would set the upper end of my range to 8KHz (not the desired 100kHz) and the resolution would of corse suffer.
I have tried using the sys_tick timer running at 1 full counter period, thinking because it is an higher priority IRQ it may help, it dose help but doesn't solve the issue.
I think I am going to get some STM32U031C6 as these are pin for pin with my L010 (with the exception of Vbat, which I have no tracks on anyway), PA0 is still TIM2 and happens to be the 32 bit timer which should negate all my current issues.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.