2021-01-27 7:52 PM
Dear Sir
My customer use STM32H750VBT6 for their product at Jan 2020. They success to program a bootloader into MCU, after boot-load, the MCU can load an application firmware into it. They produced over 10 kpcs at production line. The Date code: 004 and REV “V�?
Set up : The MCU board connected to a computer through CAN bus and computer connected to cloud and downloaded the application firmware. The application firmware was loaded to the MCU.
However, customer make a new order with same part nos "STM32H750VBT6" for their product at Jan 2021. The Date code: 041 and REV “V�?. They can only program the bootloader program to the MCU. After bootload, the MCU cannot load an application firmware into it.
Set up : same as above.
When customer use back the MCU ( Datacode : 004), the MCU board works fine again.
We found that there is a Errata (ES0396) mentioned some change. But we cannot find the root cause for this ( MCU cannot load the application firmware after bootload. )
Errata sheet - STM32H750xB STM32H753xI - STM32H750xB and STM32H753xI device limitations
Could you kindly help for us ?
Thanks a lot !!
Patrick Law
2021-01-28 3:25 AM
Where is the application firmware located?
Does your customer understand that H750 legally has only 128K of flash?
-- pa
2021-01-28 5:29 AM
Hi Pavel
Thanks for your help
1. Inside the external flash
2. Yes we are aware of that
Moreover, Do ST provide the bootloader and testing firmware to verify the bootloader process on MCU?
Thanks
Patrick
2021-01-28 6:50 AM
The error description is a bit fuzzy. "After bootload, the MCU cannot load an application firmware into it."
Are there any debug prints or other means to find where exactly it fails: copy to external flash, copy from external flash to RAM, verifying CRC or signature? ....
> Do ST provide the bootloader and testing firmware to verify the bootloader process on MCU?
ST provides several examples for external flash and RAM on H750:
-- pa
2021-01-31 7:05 PM
Dear Pavel
My customer want to handle this case directly because the system is designed by them.
Do you have a ticket number or reference nos for this case ?
So that I can pass this case number to him.
Or , how can I pass this case to my customer ?
Please advise. Thanks
Best Regards
Patrick Law
2021-02-01 7:40 PM
Hi Pavel
May I have your update ?
Thanks
Best Regards
Patrick Law
2021-02-01 10:59 PM
Community Members aren't ST Employees, you can create an online support case or work with your FAE (Support Engineer) directly.
2021-02-02 12:14 AM
Hi Tesla DeLorean
Noted.
Thanks for your reminder.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.