2018-07-13 4:29 PM
Hi,
what is the procedure to start the system bootloader in the STM32H743 via software. Even newest AN2606 is not clear on this, since none of the mentioned methods fit the STM32H7 registers etc.
What I mean:
For the F4 the system memory needs to be remapped to 0x00000000, load MSP from value in address 0x00000000 and then a jump to the address stored in address 0x0000004 is done. This works for an F4.
On the F7 (also a Cortex-M7) some option bytes have to be configured correctly and then it is basically MSP from 0x1ff0000 and jump to value of 0x1ff00004.
But what is the procedure on the H7? The system memory is located like on the F7 on 0x1ff00000 but it is not readable, and because of that no loading of MSP and reading the correct jump address. There is no system memory remapping bit in the SYSCFG register which is what AN2606 suggests to use, the only exception mentioned is for the F7. I think there is either no way to achieve this on the STM32H7 or another not yet documented way. In any case, AN2606 is lacking sufficient information, probably forgotten when adding the H7.
Just for reference: When booting with the BOOT pin high, DFU works, no problems here. It is a Rev. Y
Anyone any idea what works?
Werner
Solved! Go to Solution.
2018-07-13 8:17 PM
0x1FF09800
2018-07-13 8:17 PM
0x1FF09800
2018-07-14 12:33 AM
Original Posted on July 14, 2018 at 07:33
Definitely gets into ROM
startup.s (Keil)
Reset_Handler PROC
EXPORT Reset_Handler [WEAK]
IMPORT SystemInit
IMPORT __main
; STM32H7 Boot-to-ROM sourcer32@gmail.com 13-July-2018
LDR R0, =0x2001FFFC ; Safe End-of-RAM location (for demonstration)
LDR R1, =0xBEEFBEEF ; Special Key
LDR R2, [R0, #0]
CMP R1, R2
BNE NotDFuse
STR R0, [R0, #0] ; Invalidate Key
LDR R1, =0xE000ED00 ; SCB
LDR R0, =0x1FF09800 ; ROM BASE
STR R0, [R1, #8] ; VTOR
LDR SP,[R0, #0] ; ROM Stack Pointer
LDR R0,[R0, #4] ; ROM Program Counter
BX R0
NotDFuse
LDR R0, =SystemInit
BLX R0
LDR R0, =__main
BX R0
ENDP Reset_Handler
main.c
void DFUBoot(void)
{
*((uint32_t *)0x2001FFFC) = 0xBEEFBEEF; // Special Key to End-of-RAM
SCB_CleanDCache();
NVIC_SystemReset();
}Formatting broken in forum transition, edited to try and fix that
2018-07-14 2:17 AM
Thanks Clive,
works like a treat.
I am using the normal approach just like on the F7, see above, but with 0x1FF09800 instead of 0x1FF00000, and bingo, the DFU device reports itself on USB.
Werner
2018-07-14 7:14 AM
Yes, ST's 'Normal' method is a bit circuitous and fraught, I've been pushing this type of method for longer as it gets about as close to 'Reset Conditions' as one can realistically get.
I'm perplexed ST didn't provide details of the ROM location, didn't take me long to pin it down, but I've been doing this stuff of ever. I will probably create an annotated disassembly of this later.
All the NUCLEO-H743ZI are Rev Y, need to poke at the STM32H743I-EVAL which I think has engineering silicon (ES)
2018-07-14 9:54 AM
The EVAL board has a Rev Z
CPUID 411FC271 DEVID 450 REVID 1001
Cortex M7 r1p1The OTP/ROM area appears to be blank on the ES part
2019-01-21 7:04 AM
Hello,
In STM32H7, the base address of the system memory is different from the entry point of the bootloader.
Thus, in order to jump to the bootloader, address "0x1FF09800" should be used instead of "0x1FFF0000".
You may have a look on FAQ "Jump to Bootloader from application on STM32H7 devices".
Link:
https://community.st.com/s/article/STM32H7-bootloader-jump-from-application
Khouloud.
2019-01-21 10:43 AM
Thanks for pointing the FAQ page out to me. While the first answer was already good enough for my purpose, it is good to see some sample code which includes the proper deactivation procedure.
Werner
2019-01-21 10:47 AM
I suspect JumpToBootloader() will fail from interrupt context, or protected mode RTOS. On CM7 caching or MPU settings might also need to be considered.
2019-01-21 11:03 AM
Indeed the caches and MPU should be considered. In my bootloader I simply do not activate any of these (for exactly the above reason) but in general you're right. You may be right about the interrupt context and protected mode (at least for the later I hope you are!).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.