2024-04-03 10:03 AM
Hello everyone, I've designed a custom board with STM32H723ZG, previously based on STM32F767ZG. When I connect board with ST Link V2 prog through SWDIO, SWDCLK and GND, I get response that no target has been detected. I'm currently using ST-Link Utility software. If I desolder H723ZG and replace it with F767ZG, board works completely fine, without any issues.
What could possibly be issue, should I order ST-Link V3 prog for the H723 MCU?
Please check attached schematic of the board, MCU related stuff is on second page.
Thanks everyone in advance! :)
Solved! Go to Solution.
2024-04-03 10:32 AM
Hello,
ST-Link Utility software is obsolete. Start using STM32CubeProgrammer tool.
2024-04-03 10:32 AM
Hello,
ST-Link Utility software is obsolete. Start using STM32CubeProgrammer tool.
2024-04-03 10:42 AM - edited 2024-04-03 10:45 AM
how did you solder this chip?
are you sure all power pins are connected (soldered properly) including PA13, PA14 for debugging ?
2024-04-03 10:46 AM
Looks like recommendation from @mƎALLEm solved the issue! :)
Thanks a lot!!
2024-04-03 10:49 AM
That's good - please mark the solution.
2025-08-02 10:57 AM
Press the reset button while clicking on debug button on stm32cube ide for a second it will work and then erase the chip.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.