2020-08-17 2:35 PM
Hi,
I am using a STMH743 running an LWIP example, added in mbedTLS to the mix.
Eventually, got into a certificate parse issue,
narrowing it down:
I found that calloc failed:
(890) x509_crt_parse_der_core:
(899) x509_crt_parse_der_core: mbedtls_calloc(), crt->raw.p=NULL, len:995
Tried searching a bit on calloc failure, came up with this link:
https://www.keil.com/support/docs/4094.htm
But that appears to match ( ? ) the startup file that I do have:
;*******************************************************************************
; User Stack and Heap initialization
;*******************************************************************************
IF :DEF:__MICROLIB
EXPORT __initial_sp
EXPORT __heap_base
EXPORT __heap_limit
ELSE
IMPORT __use_two_region_memory
EXPORT __user_initial_stackheap
__user_initial_stackheap
LDR R0, = Heap_Mem
LDR R1, =(Stack_Mem + Stack_Size)
LDR R2, = (Heap_Mem + Heap_Size)
LDR R3, = Stack_Mem
BX LR
ALIGN
ENDIF
END
;************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE*****I am at a loss, how to go forward.
Can someone help ?
Thanks,
Manu
2020-08-17 3:21 PM
Replying to my own post ..
Played around with the Heap size,
This fixed the calloc() issue.
Sorry about the noise.
Thanks,
Manu
2020-08-17 3:33 PM
For others, stack and heap are defined in startup.s, the memory involved can be established via a scatter file
;*******************************************************************************
;
; Amount of memory (in bytes) allocated for Stack
; Tailor this value to your application needs
; <h> Stack Configuration
; <o> Stack Size (in Bytes) <0x0-0xFFFFFFFF:8>
; </h>
Stack_Size EQU 0x0800
AREA STACK, NOINIT, READWRITE, ALIGN=3
Stack_Mem SPACE Stack_Size
__initial_sp
; <h> Heap Configuration
; <o> Heap Size (in Bytes) <0x0-0xFFFFFFFF:8>
; </h>
Heap_Size EQU 0x2000
AREA HEAP, NOINIT, READWRITE, ALIGN=3
__heap_base
Heap_Mem SPACE Heap_Size
__heap_limit
;***************************************************************************** RW_RAM1 0x60000000 UNINIT 0x00040000 { ; RW data
*(HEAP) ; external SRAM
}
2020-08-17 11:13 PM
Thanks, Clive1
I have a faint memory, (you or someone else ?)
A mention about stack and heap requirements running a web server with and without TLS/SSL quite a while back ?
Could not find that discussion, anymore though.
Thanks,
Manu
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.