2025-09-25 6:39 PM - last edited on 2025-09-26 1:10 AM by mƎALLEm
Hello ST Community -
I am seeking to migrate a functioning HTTP Client application from a SAMD51 MCU to STM32 silicon, I have an STM32H573I-DK on hand, objectives:
Other than the demo program, I have not deeply explored the STM32H573I-DK. Any configuration, and coding tips / examples would be greatly appreciated.
Thanks much,
Kelly
Solved! Go to Solution.
2025-09-26 1:00 AM
Hello Kelly,
This is an interesting task. I can offer a suggestion on the HTTP Client side of your project.
You can use the Mongoose Networking Library. It's a lightweight library designed for embedded systems, with support for many networking protocols, and is a good fit here because it provides both a simple HTTP client and a built-in JSON parser. This means you don't need to add a separate library just to handle the retrieved objects. Mongoose is well-documented here and has a clean, non-blocking API.
You can use the following resources as a starting point:
As for your other requirements, you can use the standard STM32 HAL functions for the SD card and LCD, and integrate those calls into the Mongoose project.
Heads up: I am part of the Mongoose development team. Hope this helps you get started.
2025-09-25 7:18 PM - edited 2025-09-25 7:22 PM
Here you can find help for your STM32 project.
You can split the project to 3 parts that can be done in parallel, maybe by different people: http client, SD-card and the LCD.
2025-09-26 1:00 AM
Hello Kelly,
This is an interesting task. I can offer a suggestion on the HTTP Client side of your project.
You can use the Mongoose Networking Library. It's a lightweight library designed for embedded systems, with support for many networking protocols, and is a good fit here because it provides both a simple HTTP client and a built-in JSON parser. This means you don't need to add a separate library just to handle the retrieved objects. Mongoose is well-documented here and has a clean, non-blocking API.
You can use the following resources as a starting point:
As for your other requirements, you can use the standard STM32 HAL functions for the SD card and LCD, and integrate those calls into the Mongoose project.
Heads up: I am part of the Mongoose development team. Hope this helps you get started.
2025-09-30 6:22 PM
Thanks Pavel for providing awareness of developmental resources.
2025-09-30 6:24 PM
...will explore the Mongoose Networking Library as a supported approach. Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.