2025-10-27 7:10 AM - edited 2025-10-27 7:11 AM
Hello!
I am facing a problem when trying to connect to a remote server using NetXDuo and MQTT. We have a cloud service with which we want to establish a connection so we can send some data. I am basing my project on the example from the STMH573 MQTT Client. The exact problem I am facing is that when trying to establish the connection using the username and password, and the certificates an error occurs, when trying to secure connect. I get these two TSL alerts - alert level is 0x2 and alert value 0x28 (secure connection failed to be established). Using TLSv1.2.
What I did:
openssl x509 -in ca.crt -outform DER -out ca.der
# Then convert into the header file format using xxd.exe
xxd.exe -i ca.der > ca.cert.hopenssl x509 -in client.crt -outform DER -out client.der
# Then converting it into the header file format
xxd.exe -i client.der > client.cert.hopenssl rsa -outform der -in client.key -traditional -out client.key.der
# Then converting it into the header file format
xxd.exe -i client.key.der > client.key.h/* Before connecting, send the username and password to log in */
ret = nxd_mqtt_client_login_set(&MqttClient, MQTT_USERNAME, MQTT_USERNAME_LEN, MQTT_PASSWORD, MQTT_PASSWORD_LEN);
if (ret != NX_SUCCESS)
{
Error_Handler();
}
/* Start a secure connection to the server. */
ret = nxd_mqtt_client_secure_connect(&MqttClient, &mqtt_server_ip, MQTT_PORT, tls_setup_callback,
MQTT_KEEP_ALIVE_TIMER, CLEAN_SESSION, NX_WAIT_FOREVER);ret = nx_secure_x509_certificate_initialize(trusted_certificate_ptr,
(UCHAR*)ca_der, // Pointer to CLIENT CERTIFICATE data
ca_der_len, // Length of the CLIENT CERTIFICATE data
NX_NULL,
0,
NULL, // Pointer to CLIENT PRIVATE KEY data
0, // Length of CLIENT PRIVATE KEY data
NX_SECURE_X509_KEY_TYPE_NONE); // Type of private key
ret = nx_secure_tls_trusted_certificate_add(TLS_session_ptr, trusted_certificate_ptr);
if (ret != TX_SUCCESS)
{
Error_Handler();
}ret = nx_secure_x509_certificate_initialize(&local_client_certificate,
(UCHAR*)client_der, // Pointer to CLIENT CERTIFICATE data
client_der_len, // Length of the CLIENT CERTIFICATE data
NX_NULL, 0,
(UCHAR*)client_key_der, // Pointer to CLIENT PRIVATE KEY data
client_key_der_len, // Length of CLIENT PRIVATE KEY data
NX_SECURE_X509_KEY_TYPE_RSA_PKCS1_DER); // Type of private key
ret = nx_secure_tls_trusted_certificate_add(TLS_session_ptr, &local_client_certificate);
if (ret != TX_SUCCESS)
{
Error_Handler();
}extern const USHORT nx_crypto_ecc_supported_groups[];
extern const UINT nx_crypto_ecc_supported_groups_size;
extern const NX_CRYPTO_METHOD *nx_crypto_ecc_curves[];
ret = nx_secure_tls_ecc_initialize(TLS_session_ptr,
nx_crypto_ecc_supported_groups,
nx_crypto_ecc_supported_groups_size,
nx_crypto_ecc_curves);After all that I am still facing the same problem - unable to establish a connection. What else have I done:
Where the program fails is here -
if (client_ptr -> nxd_mqtt_client_use_tls)
{
status = nx_secure_tls_session_start(&(client_ptr -> nxd_mqtt_tls_session), &(client_ptr -> nxd_mqtt_client_socket), wait_option);
if (status != NX_SUCCESS)
{
/* Revert thread priority. */
tx_thread_priority_change(tx_thread_identify(), old_priority, &old_priority);
/* End connection. */
_nxd_mqtt_client_connection_end(client_ptr, NX_NO_WAIT);
return(NXD_MQTT_CONNECT_FAILURE);
}
}returning error code 0x114 (NX_SECURE_TLS_ALERT_RECEIVED) - The remote host sent an alert, indicating an error and closing the connection. This from the nxd_mqtt_client.c file.
I am not sure what else to do and to test. Any help or guidance is appreciated!
Solved! Go to Solution.
2025-12-05 4:36 AM
Since the last post I have fixed these issues. Just posting this so that someone, if they are ever in a similar situation or having a similar problem, can see this and hopefully find an answer or at least a direction.
For threads like MQTT and IP Instance (dealing with Ethernet and "communicating" with LAN8742 driver) thread, I have set 8KB and 12KB of stack memory, respectively. Although not sure if MQTT thread really needs 8KB of memory, but the system has been quite robust, and I am not going to change it in the near future.
I set the NX_IP_FAST_TIMER_RATE and NX_IP_STATUS_CHECK_WAIT_TIME settings to a value of 10, which solved a couple of issues regarding TCP retransmissions being sent a little too often and DNS query failing at some times. What helped also with too many TCP retransmissions being sent was setting NX_TCP_FAST_TIMER_RATE to a value of 30 (NX_IP_PERIODIC_RATE is divided with the set value to calculate the fast TCP timer rate). So, when I had the NX_IP_PERIODIC_RATE set to 1000, divided by a value of 30 would give a timer rate of about 33-34 ticks (or milliseconds). But, when leaving NX_IP_PERIODIC_RATE to the default value of 100 ticks per second, then this might not be very helpful.
All in all, how I made the MQTT project work was finding the correct balance between giving enough memory to threads and setting the system to be fast enough to be able to react.
2025-10-29 1:30 AM
I managed to fix one of the issues, which is related to adding the client certificate and the client key. The solution was using the nx_secure_tls_local_certificate_add instead of the nx_secure_tls_trusted_certificate_add.
ret = nx_secure_x509_certificate_initialize(&local_client_certificate,
(UCHAR*)client_der, // Pointer to CLIENT CERTIFICATE data
client_der_len, // Length of the CLIENT CERTIFICATE data
NX_NULL, 0,
(UCHAR*)client_key_der, // Pointer to CLIENT PRIVATE KEY data
client_key_der_len, // Length of CLIENT PRIVATE KEY data
NX_SECURE_X509_KEY_TYPE_RSA_PKCS1_DER); // Type of private key
ret = nx_secure_tls_local_certificate_add(TLS_session_ptr, &local_client_certificate);
if (ret != TX_SUCCESS)
{
Error_Handler();
}
Now, there is the issue when publishing the message, and the program gets stuck here:
/* Wait for the broker to publish the message. */
tx_event_flags_get(&mqtt_app_flag, DEMO_ALL_EVENTS, TX_OR_CLEAR, &events, TX_WAIT_FOREVER);It seems that the message has been published, but not sure why the program gets stuck here. Is it because there is still some settings missing or wrong configuration on NetXDuo side? Or is it that the remote server, that did receive the published message, did not respond for some reason?
2025-11-05 5:36 AM - edited 2025-11-05 6:17 AM
Hello!
The previous problem came from the fact that in my code I tried to subscribe to a topic that did not exist. Now, I uncommented all the code that deals with the subscribing. After that, I can send/publish messages to the remote server.
But at random times, the program just hangs and does not send anymore. When this happens I usually get the NXD_MQTT_PACKET_POOL_FAILURE (0x10006 code) error. My packet size pool is set to 20 packets. Does it mean that the packet pool will be filled at some point, due to which the system cannot handle anymore packets? If I understood NetXDuo correctly, then every time I receive the PUBACK from the remote server, the packet pool is emptied, in which case my previous assumption is incorrect.
Also, at some points the connection is dropped (I strongly believe that is caused by NetXDuo as we have another system sending MQTT packets, which does not loose the connection). But I tried to create a function that tries to reconnect, but the second time DNS function nx_dns_host_by_name_get is called, it returns an error - NX_DNS_QUERY_FAILED (0xA3).
In summary, program gets stuck at some point and not sending anymore packets or when the connection drops, and when trying to reconnect, I am unable to do so. Are these problems connected somehow or are these separate issues in my code?
All the ideas and help would be much appreciated!
Edit 1: I also noticed that in the NetXDuo section, some priorities seem to be a little off. What I mean by this is for example the NX_APP_THREAD_PRIORITY is set to 10, but MQTT_PRIORITY and SNTP_PRIORITY have these priorities - 3 and 5, respectively. Should not NX_APP_THREAD_PRIORITY have the highest priority of them all, because it deals with IP level things?
2025-12-05 4:36 AM
Since the last post I have fixed these issues. Just posting this so that someone, if they are ever in a similar situation or having a similar problem, can see this and hopefully find an answer or at least a direction.
For threads like MQTT and IP Instance (dealing with Ethernet and "communicating" with LAN8742 driver) thread, I have set 8KB and 12KB of stack memory, respectively. Although not sure if MQTT thread really needs 8KB of memory, but the system has been quite robust, and I am not going to change it in the near future.
I set the NX_IP_FAST_TIMER_RATE and NX_IP_STATUS_CHECK_WAIT_TIME settings to a value of 10, which solved a couple of issues regarding TCP retransmissions being sent a little too often and DNS query failing at some times. What helped also with too many TCP retransmissions being sent was setting NX_TCP_FAST_TIMER_RATE to a value of 30 (NX_IP_PERIODIC_RATE is divided with the set value to calculate the fast TCP timer rate). So, when I had the NX_IP_PERIODIC_RATE set to 1000, divided by a value of 30 would give a timer rate of about 33-34 ticks (or milliseconds). But, when leaving NX_IP_PERIODIC_RATE to the default value of 100 ticks per second, then this might not be very helpful.
All in all, how I made the MQTT project work was finding the correct balance between giving enough memory to threads and setting the system to be fast enough to be able to react.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.