2022-03-04 12:27 AM
HI
At what temperature the TS_CAL2 value for the STM32G431 is detected?
In the datasheet it is reported 130 degrees while in the library "stm32g4xx_ll_adc.h" TEMPSENSOR_CAL2_TEMP is 110 degrees
Thanks
Solved! Go to Solution.
2022-03-04 2:16 AM
Hello,
Correct answer is 130°C
You're probably using STM32G4 firmware package below version 1.5.0, where it is updated.
2022-03-04 2:16 AM
Hello,
Correct answer is 130°C
You're probably using STM32G4 firmware package below version 1.5.0, where it is updated.
2022-03-04 3:31 AM
Right, thanks,
For the G431 I'm using STM32CubeIDE Version 1.7.0 with STM32Cube FW_G4 V1.4.0 because using STM32CubeIDE Version 1.8.0 with STM32Cube FW_G4 V1.5.0 and the same code the interrupts are not generated or intercepted and I don't understand why
2022-03-11 2:24 AM
Hi @doubleset ,
New versions for STM32CubeIDE & STM32CUbeMX are currently available. If the issue with interrupts you introduced previously is still there, please describe it with more details in a new post. It will be helpful in order to anlayze & fix it.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-24 10:56 AM
Has this been fixed? It appears to still be incorrectly specified as 110C in STM32Cube FW_G4 V1.6.0
See https://github.com/STMicroelectronics/stm32g4xx_hal_driver/issues/20
2025-09-09 5:55 AM
I don't think it has been fixed.. Had to hardcode it to 130UL myself..
2025-09-09 7:01 AM
It is 130 and is correct in the GitHub version, but a library release has not yet been made which includes this fix.
This issue was fixed a few years ago, then broken, and now fixed but not yet released.
2025-09-18 2:14 AM
It is 130 deg.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.