2026-04-20 11:26 PM - last edited on 2026-04-23 4:01 AM by Andrew Neil
Hi all.
I wish disable auto PAD disable CRC append.
Send packet use low_level_output(), before call HAL_ETH_Transmit_IT()
I set
TxConfig.ChecksumCtrl = ETH_CHECKSUM_DISABLE;
TxConfig.CRCPadCtrl = ETH_CRC_PAD_DISABLE;but packet allways pad to 60byte,
if use TxConfig.CRCPadCtrl = ETH_CRC_PAD_DISABLE;, no packet output
if use TxConfig.CRCPadCtrl = ETH_CRC_INSERT; output fine but have 4byte crcr append.
How to do , NO-PAD NO-CRC send packet?
2026-04-23 3:47 AM
Hello @mings_chihs, and Welcome to ST Community!
With the STM32F7 Ethernet MAC, a normal Ethernet transmission is expected to include padding to 60 bytes and a 4-byte CRC/FCS. A frame with both NO-PAD and NO-CRC is generally invalid on Ethernet. Therefore, if the frame is shorter than the Ethernet minimum length, the MAC or network will not treat it as a valid packet.
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.