2019-04-30 2:03 AM
Hello,
i have a Nucleo-144 board, where i replaced the STM32F429ZI for a STM32F439ZI.
I used CubeMX 5.2.0 to create a ethernet test project just to ping the board and go further from there, but i cant get it to work.
Ethernet is enabled
Ethernet interrupt is enabled.
The parameter settings:
And the advanced parameter settings:
The clock configuration:
LwIP is enabled, general settings (Ive tested with bot static and dynamic IP, both wont work):
I left most of the LwIP options at standart, except i set
LWIP_BROADCAST_PING (Respond to Broadcast Pings) Enabled
LWIP_MULTICAST_PING (Respond to Multicast Pings) Enabled
Also CHECKSUM_BY_HARDWARE is enabled, as well as all the CHEKSUM_GEN_*** and CHECKSUM_CHECK_***
Ive build the source code with Minimum Heap Size 0x2000 and Minimum Stack Size 0x4000.
In Atollic TrueSTUDIO 9.0.1 ive build the project, where i needed to copy fsdata.c to Middlewares/Third_Party/LwIP/src/apps/httpd/ and exclude it from build, so the file would build properly.
I added MX_LWIP_Process(); to the while(1) in main.c, compiled and flashed the board.
At this point i should be able to ping it already, but i get no response whatsoever.
It doesnt matter if i use a crossed or straight ethernet cable, connect it to the network or directly to the PC and if i give a static or dynamic IP, i cant ping the board at all.
Im in a dead end with this, i suspect that the F439ZI MCU on a F429ZI nucleo board wont work, but at this point i dont know what could be wrong. Any tipps/help would be appreciated.
Solved! Go to Solution.
2021-01-05 8:25 AM
Hi,
I'm facing the problem to connect the Ethernet to STM32F439ZT nucleo board.
but i'm not able to connect it.i given all configuration
like
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "lwip.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "lwip/apps/httpd.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart3;
PCD_HandleTypeDef hpcd_USB_OTG_FS;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_USB_OTG_FS_PCD_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_USB_OTG_FS_PCD_Init();
MX_LWIP_Init();
/* USER CODE BEGIN 2 */
// initializing the HTTPd
httpd_init();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
MX_LWIP_Process();
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
can you please suggest any one.
thank you.
2021-01-08 2:06 AM
Hello
The iformation you provide is not enough to understand the problem
With this configuration, eth. cable must be connected to board before program start
In case you use DHCP, try a delayed start of httpd_init(), not to conflict with DHCP transactions
//##############################################################################
void TimeoutHTTPDHandler(void*arg)
{
httpd_init();//init
// http_set_ssi_handler(SSI_Handler, TAGS, num_tags);//set callbacks for SSI array
// http_set_cgi_handlers(CGI_TAB, 1);//set callbacks for CGI array
}
//##############################################################################
in main.c file
sys_timeout(4000, TimeoutHTTPDHandler, NULL);// for delayed start of HTTPD server
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.