2017-08-17 2:30 AM
Hello everyone, I am new to the forum.
Currently I am busy working on a project that must use USB communication.
I therefore implemented the USB VCP library for a STM32F437 microcontroller.
I am able to communicate and receive data in USB from a PC.
Unfortunately, I encounter a problem when I try to send a lot of data continuously. The program switches to hardfault handler after a few seconds of transmission.
I use the VCP_DataTx function.
Uint16_t VCP_DataTx (uint8_t * Buf, uint32_t Len)
{Uint32_t i;Pour (i = 0; i <Len; i ++) {
APP_Rx_Buffer [APP_Rx_ptr_in ++] = * (Buf + i);}/ * Pour �viter le d�bordement du tampon * /
Si (APP_Rx_ptr_in == APP_RX_DATA_SIZE) {APP_Rx_ptr_in = 0;}Retour USBD_OK;
}I was able to read some posts on different forums concerning a problem coming from the library.
Have you solved this type of problem? Do you have any examples?
Thank you for your reply
#usb-datatx2017-08-18 10:29 AM
If you don't mind, I will change the French keywords to the standard C ones. The problem here is a typical buffer overflow, which can be fixed by correctly placing the circular buffer index reset inside the for loop.
Uint16_t VCP_DataTx (uint8_t * Buf, uint32_t Len)
{ Uint32_t i; for (i = 0; i <Len; i ++) { APP_Rx_Buffer [APP_Rx_ptr_in ++] = * (Buf + i); / * Pour éviter le débordement du tampon * / if (APP_Rx_ptr_in == APP_RX_DATA_SIZE) { APP_Rx_ptr_in = 0; } } return USBD_OK;}2017-08-22 4:49 AM
Thank you for your reply.
Unfortunately the problem is still the same.
Could the problem come from a parameter in my CDC configuration?
#define USBD_CFG_MAX_NUM 1
#define USBD_ITF_MAX_NUM 1#define USB_MAX_STR_DESC_SIZ 255
#define CDC_DATA_MAX_PACKET_SIZE 64 /* Endpoint IN & OUT Packet size */
#define CDC_CMD_PACKET_SZE 8 /* Control Endpoint Packet size */#define CDC_IN_FRAME_INTERVAL 5 /* Number of frames between IN transfers */
#define APP_RX_DATA_SIZE 2048 /* Total size of IN buffer:The Baudrate of my communication is 19200bit/s.
When there is an overflow, the USB port jumps and the processor goes into hardfault handler.
Would it be possible to re-establish communication?
Thank you for your reply
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.