2022-07-17 11:15 PM
Hi. I am using STM23L031 for a battery operated product. The expected life cycle is almost 1 year so I need to save battery as much as possible. So I wanted to use Low power sleep mode when not doing anything(I chose this because I need DMA for UART which is always ON since I receive data over UART). Also I have 3 input interrupts over GPIO pins.
Basically, when I am in run mode, I want to run the controller at 32MHz (even after exiting low power mode, I want to switch the frequency to 32MHz).
So, when entering Low power sleep mode I did this as per the datasheet:
But when I exit from Low power mode, I get Hard Fault.
Any reason why this is happening? And how to overcome this problem?
Here is my main() function:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config_32MHz();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_LPUART1_UART_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
enter_low_power_sleep_mode();
SystemClock_Config_32MHz();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}And here is my enter_low_power_sleep_mode() function:
void enter_low_power_sleep_mode(void)
{
__HAL_FLASH_SLEEP_POWERDOWN_ENABLE();//switch off flash memory
SystemClock_Config_131KHz();//configure clock for 131kHz
SET_BIT(PWR->CR, PWR_CR_LPSDSR);
CLEAR_BIT(SCB->SCR, SCB_SCR_SLEEPDEEP_Msk);//low power mode = sleep mode(clear deep sleep bit)
__WFI();
}NOTE: SystemClock_Config funcitons are autogenerated using STM32CubeIDE.
Also, any examples which I can refer for doing the same?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.