2014-10-26 12:01 PM
Hi,
I am looking for some info regarding the external clock bypass conditions for STM32F417IG. There was not sufficient info in the datasheet. But, in the reference manual I could find some related data regarding how it can be done. Another problem was the Clock Config tool does not support the external clock bypass conditions. So, that was a problem in generating the required related C code to dump. I just wanted to confirm if the following changes in the system_stm32f4xx.h header file would be sufficient to use the chip in bypass conditions by feeding it using an external single ended clock source and have it communicating with the computer with VCP: I set it to pll_source_hse_bypass. and RCC->CR |= ((uint32_t)(RCC_CR_HSEON | RCC_CR_HSEBYP)); RCC->CR |= ((uint32_t)RCC_CR_HSEON); In the main.c: I have the following config- &sharpdefine HSE_VALUE((uint 32_t)8000000) should I leave it as it is or make any changes to this in main? I request you to please provide any other samples/code/reference design if available about the same conditions. I already tried with the modifications mentioned above and I think I partially bricked one of the device. I am able to program the flash but it is not able to communicate with pc as the VCP is not being detected. I thereby request you to please look into this and provide some solutuon. Thanks, Sa #stm32f417 #stm32f417 #stm32f417 #hse-hsi-pll-rcc #vcp-stm32f4 #rtfm #external-clock #hse-config2014-10-27 1:33 PM
Thanks for the explanation. I will limit the hse to <50 mhz.
Also, an update(just found out): The workaround for using clock config tool in hse bypass conditions is to set the HSE_VALUE to the HSE bypass oscillator's frequency.2014-10-27 1:49 PM
I'm not sure if the PLL is the limiting factor here or not, you'd have to find someone who understood the critical paths in the design. ST indicate 50 MHz is where it was designed to work, but not tested in production. I'd assume the 50 MHz number relates to Ethernet PHY clocking sources.
The PLL's VCO wants to dwell in the 192 to 432 MHz range, they want the PLL comparison frequency at 1 to 2 MHz, and the M Divider has 6-bits with suggested range of 2-63. If that divider/counter works at high speeds, one might be able to push 126 MHz. The N Divider is bigger and capable of 432 MHz operation. One could presumably experiment with the corners of this design over frequency, voltage and temperature. I don't know of anyone who's does such a characterization. For generating other frequencies, there is the I2SPLL with output via MCO22014-10-27 1:54 PM
I'll note that you can run the CPU directly from HSE, and still run the PLL to generate the 48MHz for SDIO, USB, etc.
2014-10-27 2:23 PM
When you say the M-divider can be modified to push to 126 Mhz. All this is internal, right? We cannot send in a higher freq than 50 and increase this 126 to even higher value.
50 MHz is for single ended sources and 26 MHz for external crystals. I think PLL is the critical block here because. If the pll is bypassed then the external clock can control the chip and peripherals(if they can handle high frequencies).2014-10-27 4:40 PM
The node you're trying to clock for the CPU and peripheral divisors (APB1/APB2) is rated to 168 MHz.
What I'm suggesting is that the PLL gearing *MIGHT* be able to get to 126 MHz, as 126 MHz DIV 63 = 2 MHz which is the top end of the comparison frequency range for the PLL, with the maximal divisor.2014-10-29 4:14 PM
Clive,
For HSE bypass clock of 50 MHz these are the changes made-//In the PLL parameters
#define PLL_M 25
#define PLL_N 336 #define PLL_P 168 #define PLL_Q 14//In the SetSysClock fn
RCC->CR |= (uint32_t)(RCC_CR_HSEON | RCC_CR_HSEBYP); In main.c #define
HSE_VALUE((uint 32_t)50000000) But, the USB is not being recognized when I plug the 50 Mhz clock and power it up. Do you think any change required? Thanks2014-10-29 4:37 PM
#define PLL_M 50
#define PLL_N 336 #define PLL_P 2 #define PLL_Q 72014-10-29 5:37 PM
Clive,
No change even with the parameters you mentioned. I also tried lowering the frequency from 50 Mhz but still same case2014-10-29 7:37 PM
Perhaps the problem is some place else?
Attached is a VCP example that should work at 50 MHz ________________ Attachments : core417i_50mhz_vcp.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzP7&d=%2Fa%2F0X0000000bLO%2FUhcXjQKVEYqo7Unj.e2B97sBirv5i8LR3wsF0vVUu_w&asPdf=false2014-10-29 7:50 PM
Clive,
Thanks for the file I flashed the hex file you provided. and gave a 50mhz clock on ph0 pin. It still does not enumerate It is only able to enumerate in normal clock conditionWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.