2014-11-05 7:20 AM
Hi All
I'm working on a project which needs to send few standard USB Keybord commands to a WIN7 Desktop. It is very simple project I'm using F103 and the ST USB library and everything seems to be working fine. When I plug the USB cable into the PC, the device gets enumerated correctly and everything works perfectly. The problem starts if I switch off and on the PC with the USB cable still plugged in - the device is not enumerated at all - I have to unplug the device and plug it back in for it to start working again. I was hoping that someone had come accross something simillar and could shed some light on this mystery. Thanks in advance. Marek #stm32 #usb2014-11-06 8:04 PM
To answer to your question, more information is required.
a) Power source - bus-/self-powered Is your USB device powered by the USB 5V line (VBUS)? - bus-powered OR Does it have a dedicated power source like a battery? - self-powered b) D+ Pull-up - fixed or controlled Does the D+ pull-up resistor (1.5k Ohm) connect directly to 3V3 (or 5V) rail? - fixed OR Is this resistor driven by a transistor (FET) or one of MCU port? - controlled TsuneoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.