2016-06-08 6:51 AM
Hello,
I have configured USART2 to communicate as RS422. Rx is connected to PA.3, Tx to PD.5. I need baudrate 921.600 Baud. There is no problem send anything one or more bytes. I can not receive anything from Rx (PA.3) pin, but when I sent anything, RXNE pin is set toghether with IDLE and ORE. DR register contain 0x7F. I sent 0x55. Situation is same if I have or not data on Rx line (0x55 from the other micro). Is there somebody who could give me an advice, where may be a problem (where is devil lie). Thanks Jiri #no-hablo-hal2016-06-08 7:15 AM
Provide a complete/concise example of the code that should demonstrate this. I've dealt with a lot of USART issues, but not looking to play 20 question to pull out the detail.
How does the configuration for using a differential pair for each channel alter the configuration of the USART?2016-06-08 9:52 PM
Hi, there is my code. Rx and Tx wires are connected to ISL3176EIUZ driver.
// ----------------------------------------------------------------------------------- // copy from the hal.h and hal.c // RS422 TXD #define HAL_422TxPort GPIOD #define HAL_422TxPin GPIO_PIN_5 #define HAL_422TxAf GPIO_AF7_USART2 // RS422 RXD #define HAL_422RxPort GPIOA #define HAL_422RxPin GPIO_PIN_3 #define HAL_422RxAf GPIO_AF7_USART2 // RS422 EnRx #define HAL_422EnRxPort GPIOD #define HAL_422EnRxPin GPIO_PIN_3 // RS422 EnTx #define HAL_422EnTxPort GPIOD #define HAL_422EnTxPin GPIO_PIN_4 // enable clocks are on the different place // RS422_TXD GPIO_InitStructure.Pin = HAL_422TxPin; GPIO_InitStructure.Alternate = HAL_422TxAf; HAL_GPIO_Init(HAL_422TxPort, &GPIO_InitStructure); // 422_RXD GPIO_InitStructure.Pin = HAL_422RxPin; GPIO_InitStructure.Alternate = HAL_422RxAf; HAL_GPIO_Init(HAL_422RxPort, &GPIO_InitStructure); // outputs HAL_422EnRxPort->BSRRH = HAL_422EnRxPin; // set to 0 ... enabled HAL_422EnTxPort->BSRRH = HAL_422EnTxPin; // set to 0 ... dissabled GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStructure.Speed = GPIO_SPEED_HIGH; GPIO_InitStructure.Pull = GPIO_NOPULL; GPIO_InitStructure.Pin = HAL_422EnRxPin; HAL_GPIO_Init(HAL_422EnRxPort, &GPIO_InitStructure); GPIO_InitStructure.Pin = HAL_422EnTxPin; HAL_GPIO_Init(HAL_422EnTxPort, &GPIO_InitStructure); // ----------------------------------------------------------------------------------- USART_HandleTypeDef husart2; /* USART2 init function */ void MX_USART2_UART_Init(void) { __USART2_CLK_ENABLE(); husart2.Instance = USART2; husart2.Init.BaudRate = 921600; //2457600; husart2.Init.WordLength = USART_WORDLENGTH_8B; husart2.Init.StopBits = USART_STOPBITS_1; husart2.Init.Parity = USART_PARITY_NONE; husart2.Init.Mode = USART_MODE_TX_RX; // huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; // huart2.Init.OverSampling = UART_OVERSAMPLING_16; husart2.Init.CLKPhase = USART_PHASE_1EDGE; husart2.Init.CLKPolarity = USART_POLARITY_LOW; husart2.Init.CLKLastBit = USART_LASTBIT_DISABLE; HAL_USART_Init(&husart2); } // ----------------------------------------------------------------------------------- MX_USART2_UART_Init(); HAL_422EnTxPort->BSRRL = HAL_422EnTxPin; // set to 1 ... enabled while (1) { if ((USART2->SR & USART_FLAG_RXNE) != 0) { RxBuf2[0] = USART2->DR; USART2->DR = 0xAA; while ((USART2->SR & USART_FLAG_TXE) == 0) {osThreadYield();} USART2->DR = RxBuf2[0]; while ((USART2->SR & USART_FLAG_TXE) == 0) {osThreadYield();} } //HAL_USART_Transmit(&husart2, RxBuf2, 1, 1); //osThreadYield(); USART2->DR = 0x55; while ((USART2->SR & USART_FLAG_TC) == 0) {osThreadYield();} osDelay(1); } that's all Jiri2016-06-08 10:09 PM
Hi. There are two screenshots from osciloscope.
With active and with calm Rx line. On the othere side of line is STM32F429 and same driver ISL3176 connected to USART6. There is no problem send or receive datas. Jiri ________________ Attachments : Active_Rx.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0kf&d=%2Fa%2F0X0000000bdF%2FfUOkAduaJ4_XXBgxdzzH05oiv0t9Am3BeHrHuy.ZFrM&asPdf=falseCalm_Rx.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0ka&d=%2Fa%2F0X0000000bdG%2Fp7_or0Ad2pV1xx6L_0tyzNsIeN8fX2syQahDmmgK8io&asPdf=false2016-06-08 10:24 PM
Better Active_Rx.jpg
________________ Attachments : Active_Rx.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0kL&d=%2Fa%2F0X0000000bdD%2FE2q2eRk0TVLThqAJ7oucYqHfNvQd0b1kTpseifEfVDw&asPdf=false2016-06-08 11:56 PM
If Rx does not react on real incoming data, and does react on Tx-ing, it then does not matter what is connected and what are the waveforms, isn't it.
Post the USART registers' content. JW2016-06-09 3:11 AM
2016-06-13 2:11 AM
You have USART_CR2.CLKEN set. That implies synchronous mode.
JW2016-06-15 5:54 AM
Thank you Mr. Waclavek Jan
Reason was a using of HAL_USART library, but there is necessary to use HAL_UART library. Thank for help. JiriWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.