2019-06-12 2:24 AM
I have start from scratch to enable the CDC (VCP) .
Complie is ok.
But if i connect the board to the LapTop i get Code43.
Configuration:
STM32CubeIDE
Version: 1.0.0
Build: 2872_20190423-2022 (UTC)
Windows 10 X64
If have inserted into CDC_Control_FS
the getter an setter Methods for baudrate etc.
What should i do
2019-06-12 2:34 AM
Additional Information:
FS
Device Only
Vbus disabled
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.