2018-01-22 6:33 AM
Hello guys,
I'm using STM32F446 along with ST's USB library in a project with USB CDC class. The USB used is the FS one. What I would like to do is detect the end of a USB connection (not based on VBUS). I was wondering if this is possible and how because it seems to me that it is not. The CDC_Init_FS is never entered upon removal of the USB cable. If I take a closer look in the IRQ, I see that the Resume and Suspend interrupts are entered infinitely (Suspend then Resume, then Suspend, etc).
Did any one else have this problem?
Best regards,
Sebastian
#usb-fs #stm32-f4We’re moving the ST Community to a new platform to give you a better and more reliable community experience.