2018-12-13 11:59 PM
I have generated USB CDC code using STM32CubeMX with firmware 1.7.0. When I run the code, nothing is detected on the PC. I have disabled VBUS sensing and made sure USB peripheral Clock is enabled. I am using external 25MHz crystal and verified by PLL settings with the examples provided. When the board is not connected to PC, I continuously receive Reset interrupts but when I connect the cable, the interrupts are no longer hit. Please help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.