2014-05-24 8:11 PM
On the NUCLEO-F401RE, using the SystemClock_Config() funtion from the STM32F4xx-Nucleo template from the following file:
STM32Cube_FW_F4_V1.1.0\Projects\STM32F4xx-Nucleo\Templates\Src\main.c I cannot get the HSI calibration trim value to change with the value in the following line (line 125):RCC_OscInitStruct.HSICalibrationValue = 16;
I have tried all values from 0 to 31 and the actual HSI does not change, as determined by reading the RCC->CR and measuring the baud rate on the output from the USART2 Tx pin. However, after the MCU initialization is complete, if I attempt to change the HSI calibration trim using the __HAL_RCC_HSI_CALIBRATIONVALUE_ADJUST() macro, I can successfully change the HSI clock rate, again as determined by reading the RCC->CR and measuring the baud rate on the output from the USART2 Tx pin. Is it possible the PLL configuation changes made later after the __HAL_RCC_HSI_CALIBRATIONVALUE_ADJUST() macro call in HAL_RCC_OscConfig() function in stm32f4xx_hal_rcc.c affect the HSI calibration trim setting? It appears the HSI calibration trim is always being set to 16, the same as the value in the template.NUCLEO-F401RESTM32F401RE
CPU ID: 0x410fc241 Implementer : 0x41 Variant : 0x0 Constant : 0xf PartNo : 0xc24 Revision : 0x1 MCU ID: 0x10006433 Revision : 0x1000 Device : 0x433 HAL Version: 0x01000000 CMSIS Version: 0x02000000 #hsi #rcc #cubef4 #stm32cubef4-nucleo #hal2014-05-29 2:33 AM
Hi,
A limitation on the STM32CubeF4 HAL RCC driver is already reported consists in calibrating the HSI oscillator when it is used as system clock without stopping it, which is not allowed using the current F4 HAL RCC driver because we need to switch the system clock to another source to allow the HSI oscillator calibration.This feature will be implemented in next HAL version planned early July.With regards.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.