2017-04-11 5:49 AM
Hi,
I have downloaded STM32Cube_FW_F3_V1.7.0 and I'm trying to build examples using 'System Workbench for STM32'. I have STM32F303 Nucleo 144 Development Board (F303ZE).
I'm trying the following example:
STM32Cube_FW_F3_V1.7.0\Projects\STM32F303ZE-Nucleo\Examples\UART\UART_Printf\SW4STM32\STM32F303ZE-NucleoI imported the project in System Workbench but the project does not build. It gives error:
make all
make: *** No rule to make target `all'. Stop.* Are these example projects tested and verified to work with System Workbench?
* Is there any known bug with these examples?* How to import the project into System Workbench? May be the way I import is wrong.
In my own custom project printf/UART is not working. So I'm trying to get this example to work such that I can use it as a reference.
Any inputs might be of help to me.
Regards, Pj
#uart #stm32cube_fw_f3Solved! Go to Solution.
2017-04-12 5:45 AM
Hi
J.Prasant
,Please refer to this link
https://community.st.com/0D50X00009XkfDjSAJ
-Nesrine-
2017-04-11 6:44 AM
Hi
J.Prasant
,I'am not able to reproduice your issue using
SW4STM32 V1.0
SW4STM32/eclipse
version are you using?http://www.openstmorg/Importing+a+STCubeMX+generated+project
-Nesrine-
2017-04-12 1:25 AM
Hi
ELMHIRI.Syrine
,Thanks for your response.
I'm able to build projects generated by STCubeMX with SystemWorkbench.In my projectUART/printf is not working. The project builds and get loaded on to the STM32F303 Nucleo 144 board but Uart does not work. Its very likely there is a bug in my software. I can check MCO pins and also change LEDs on my board but Uart is not working.
As my own project isnot working I started looking out for reference code and examples. I would like to try out UART_Printf example in STM32_Cube_F3 using 'System Workbench' and but the example project provided by STM does not build.
Could you please build UART_printf example from:
STM32Cube_FW_F3_V1.7.0\Projects\STM32F303ZE-Nucleo\Examples\UART\UART_Printf\SW4STM32\STM32F303ZE-Nucleo
Using SystemWorkbench (SW4STM32 v1.0) and confirm whether it builds or not?
Regards,Pj
2017-04-12 4:13 AM
Hi
J.Prasant
,STM32Cube_FW_F3_V1.7.0\Projects\STM32F303ZE-Nucleo\Examples\UART\UART_Printf\SW4STM32
-Nesrine-
2017-04-12 5:22 AM
Hi
ELMHIRI.Syrine
,Thanks for that info. This confirms I may be doing something wrong. But I'm just importing the project and trying to build and it fails. Not sure why it is not building.
I'm looking at the example to figureout how is printf linked to USART3. If I want to use UART4 instead of USART3 for printf where should I make this change (assuming I have setup UART4 pins and clocks correctly) ?
Regards, Pj
2017-04-12 5:39 AM
Update:
I see that this code makes the connection between printf and USART3:PUTCHAR_PROTOTYPE
{ HAL_UART_Transmit(&UartHandle, (uint8_t *)&ch, 1, 0xFFFF);return ch;
}I somehow overlooked this function in main.c
Anyway.. in my project UART is working (I can send characters over UART using HAL_UART_TRANSMIT) but printf still does not work... even though I have defined the above function in my project and also defined PUTCHAR_PROTOTYPE.
Not sure what is the missing from my project.
Regards, Pj
2017-04-12 5:45 AM
Hi
J.Prasant
,Please refer to this link
https://community.st.com/0D50X00009XkfDjSAJ
-Nesrine-
2017-04-12 6:03 AM
Hi
ELMHIRI.Syrine
,Thanks for your response. From Ac6 forumsI found out that syscalls.c was the last missing thing from my project. I copied that from the example project into my project and printf started working.
Thanks for your help!
Regards, Pj
2018-12-18 12:21 AM
pls. refer to the below blog:
https://stackoverflow.com/questions/12574187/eclipse-cdt-no-rule-to-make-target-all
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.