STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Code Isolation for Functional Safety

HI,  I am considering the use of STM32F0 device for my project. How do I isolate the safety related code(for functional safety)  from the general code, so that a f/w update on the general code doesn't affect the safety related code? Are there any har...

arthiJan by Associate II
  • 8308 Views
  • 18 replies
  • 1 kudos

Trying to get Nucleo-F042K6 into DFU mode

I'm developing an application for the F042 series chips. I'm using Nucleo-F042K6 for development.I want to allow users to flush firmware using DFU mode. I am unclear on how to force the device into the DFU bootloader. Some material I read suggests th...

AKrup by Associate II
  • 2392 Views
  • 5 replies
  • 0 kudos

Mass store device for the STM32F7VIT device.

Hi, We are using the STM32F7 device and we interfaced the NAND fash device through the SPI to the controller. Now we want to access the NAND flash device through the PC directly by using the FAT file system . Without using the device drivers in PC...

MANISH by Associate II
  • 2477 Views
  • 4 replies
  • 0 kudos

Resolved! Hi, In a custom board I've the STM32F722 connected to a 8GB eMMC with a 24Mhz clock. I'm having issue reading (sigle or multiple block ) with the DMA using the HAL_MMC_ReadBlocks_DMA function.

STM32F722STM32CubeF7 Firmware Package V1.11.0 / 23-February-2018.Hi,In a custom board I've the STM32F722 connected to a 8GB eMMC with a 24Mhz clock.I'm having issue reading (sigle or multiple block ) with the DMA using the HAL_MMC_ReadBlocks_DMA func...

I want ST offer a interface HAL_UART_DMAStop_RX

I use stm32cubemx. And in stm32fxxx_hal_uart.c. There is a function "HAL_UART_DMAStop". This function will stop both TXDMA and RXDMA.But I have a request. I often use "HAL_UART_DMAStop"+"HAL_UART_Receive_DMA" to flush dma buffer. But HAL_UART_DMAStop...

STM Virtual Comm Port (VCP) driver slow on Windows 7

I have an STM32F4 device that uses the USB peripheral and CDC driver.I have a portable python app that communicates with the STM32F4 from Mac OS X 10.13 (High Sierra), Win10 and Win7.On Mac and Win10 the app communicates with good speed, however on W...

BSimo by Associate
  • 909 Views
  • 0 replies
  • 0 kudos

Bug on SDcard and stm32f415 ?

Hi, i have a problem with my project....I'm using Fat and SD with freertos to read/write files on SD using hdma channel.First part i fixed all "SDIO_STA_STBITER" with "SDIO_STA_STBITERR" (with 2 "R" ) because a typo is present.But i see the interrupt...

Marco1 by Associate II
  • 4554 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.