2025-11-03 12:05 PM
Hello, I'm having problems with a simple task: receive blocks of data from UART. The blocks are sequences of 1-300 bytes, that are receiveid with a 1 second interval. The value is stored in one buffer of 350 bytes.
When I send a big block of 270 bytes after other blocks(of 60 bytes by example) in that 1s interval, the Stm32 RESETS! But if the interval is longer, like 5 seconds, it doesn't reset and receive the data correctly.
I tried with pooling and interruption, the result is the same. I'm using 115200 baud. Lowering the baud rate also reduces the interval that doesn't cause a reset, but I can't use this solution.
WatchDog is already disabled. By this moment, the code doesn't do anything more.
Solved! Go to Solution.
2025-11-05 11:18 AM
Good catch!
Please mark the solution.
This is always a problem with using the debugger from a dev kit - there may still be connections from the dev kit, and they can affect your external target.
I would strongly recommend that you get a standalone debugger.
Failing that, you can break off the ST-Link part of the Nucleo board - so ensure no "phantom" connections.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.