2024-06-03 12:57 AM - last edited on 2025-11-05 8:33 AM by mƎALLEm
Hello,
I have managed to generate a IP through the LWIP in the STM32 IDE and establish a connection via Ethernet, although now when I upload the files from hasseb/stm32h7_atsame70_ptpd: IEEE 1588 PTP daemon for STM32H7 and ATSAME70 (github.com)
I seem to have a large portion of the code in the main.c file greyed out.
As well, I'm not sure if it is concerning that there is a warning saying "_gettimeofday is not implemented and will always fail". I found some documentation stating this is not too much of a concern, as it's only a warning and not an Error.
Furthermore, I have tried getting an output using this function just as a test and no luck:
__weak HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority)
{
/*configuring the SysTick to have an interrupt in 1ms time basis*/
HAL_SYSTICK_Config(SystemCoreClock /1000);
/*Configure the SysTick IRQ priority */
HAL_NVIC_SetPriority(SysTick_IRQn, TickPriority ,0);
/* Return function status */
return HAL_OK;
}
Thank you!
Solved! Go to Solution.
2024-06-04 10:39 AM
Hello @Gianni7315 ,
In fact, the example you are following is supporting PTP with a software implementation but on your product, it can be sone by Hardware which support this feature more details on this can be found in the reference manual section 58.5.4 IEEE 1588 timestamp support have a look especially at the explanation of PTP timestamp offload function in this section.
Regards
2024-06-04 10:39 AM
Hello @Gianni7315 ,
In fact, the example you are following is supporting PTP with a software implementation but on your product, it can be sone by Hardware which support this feature more details on this can be found in the reference manual section 58.5.4 IEEE 1588 timestamp support have a look especially at the explanation of PTP timestamp offload function in this section.
Regards
2024-06-04 11:56 PM
@STea :
the H7 hardware PTP support is looking really good, but even better would be an example from ST to make this actually work.
I'm using an adapted version of the PTPd mentioned above, started with that on an F767, then migrated it to H7, but have no time to change it using more of the H7 hardware features.
2024-06-05 4:11 AM
Hello @LCE ,
Thank you for your request and constructive feedback. I will try to make a quick guide on the setup of PTP using the Hardware features stay tuned.
regards
2025-04-28 12:34 PM
Was it already possible to create a quick guide how to setup the PTP in hardware?
2025-05-19 2:37 AM
One more request for at least "a quick guide on the setup of PTP using the Hardware features"!
2025-11-05 8:06 AM
hello @STea
i am looking into this now and would love the guide if it is aviable?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.