2026-04-16 2:03 AM - last edited on 2026-04-16 2:52 AM by Andrew Neil
I am using the STM32L433 MCU and both the HID and VCP interfaces are not working even though the DFU is.
I am simply using the STM32CubeMX software to generate a standard default USB Setup but I keep getting the same Windows USB Error "USB Device Not Recognised" which is the "Device Descriptor request failed".
My hardware is a custom design and believe that I have the correct differential impedance or the DFU would not have worked.
VBUS is at 3.3V (<4V)
D+/D- traces > 2 inches but differential impedance has been matched to 90 Ohms using Altium.
I have a 12MHZ Crystal, the MCU can run Crystal-less.
USB is 48MHz but runs from RC, also used PLLSA1 from HSE.
STM32CubeIDE v2.1.1
MX_USB_DEVICE_Init() called.
If the DFU is working then why not the other USB Interfaces?
2026-04-16 2:30 AM
2026-04-16 3:50 AM
I have followed that tutorial and all appears well.
The initialisation functions in USB_Device_Init() throw up no errors but does not continue to enumerate the device and send the descriptors.
2026-04-16 4:17 AM
@dave_mcc wrote:My hardware is a custom design
So please show the schematic.
How to write your question to maximize your chances to find a solution
@dave_mcc wrote:If the DFU is working then why not the other USB Interfaces?
By "DFU", do you mean the USB System Bootloader ?
If so that suggests that your hardware is OK - so the problem must be in your software.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.