STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 USB HID + VCP not working but DFU is

I am using the STM32L433 MCU and both the HID and VCP interfaces are not working even though the DFU is.I am simply using the STM32CubeMX software to generate a standard default USB Setup but I keep getting the same Windows USB Error "USB Device Not ...

dave_mcc by Associate
  • 258 Views
  • 3 replies
  • 0 kudos

FileX SD card insertion/removal handling

Hi,how am I supposed so handle the reinsertion event while using the FileX with an SD card? All the examples I saw assume the SD card cannot be ejected while in use which is obviously unrealistic.I tried to do it according to the official docs and wh...

Pajaka by Associate III
  • 5410 Views
  • 10 replies
  • 2 kudos

Resolved! UART Interrupts With Nucleo-L476

I have looked https://community.st.com/t5/stm32-mcus/implementing-uart-receive-and-transmit-functions-on-an-stm32/ta-p/694926 and https://wiki.st.com/stm32mcu/wiki/Getting_started_with_UART#Configure_UART_Interrupt and tested sending tx data with a S...

cbarb2747 by Associate III
  • 405 Views
  • 4 replies
  • 2 kudos

Resolved! HAL_Delay - out by 1ms ?

Hello, I am using HAL2 and wrote the basic code below: while (1) { HAL_GPIO_TogglePin(LD1_PORT, LD1_PIN); HAL_Delay(1); } I looked at the pin with an oscilloscope and I see that the signal stays 2ms low and 2ms high. If I change the code t...

USB Device CDC ACM

Hello,I am working on USB device CDC ACM for STM32N655L0. I found an example about "Ux_Device_CDC_ACM" for NUCLEO-N657X0-Q. Can I use this example for my mcu? How can I find ioc configuration of this example?I also tried to implement this example to ...

BKaya_0-1750430697260.png
B.Kaya by Associate III
  • 1337 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.