2024-11-18 11:32 AM - edited 2024-11-18 2:35 PM
I am using SPI to communicate between STM32H7B3I-DK (master) and Nucleo-H743ZI(Slave). My Data transmits as expected; however, after transmission the MISO and MOSI lines stay high. I have Master Keep IO State Enabled on both.
I am not using HW NSS, and have setup my own NSS(nCS)
SLAVE SPI:
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_SLAVE;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 0x0;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi1.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
[ISRs]
// /CS handler
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
if (GPIO_Pin == GPIO_PIN_14) {
if(HAL_GPIO_ReadPin(nCS_GPIO_Port, nCS_Pin) == GPIO_PIN_RESET){
txBuffer = pPacketSlave->ProcessCS(true); //prep transmit 0 for first byte
__HAL_SPI_ENABLE(&hspi1); //begin SPISetup
__HAL_SPI_ENABLE_IT(&hspi1, SPI_IT_RXP | SPI_IT_TXP);
__HAL_SPI_CLEAR_OVRFLAG(&hspi1);
__HAL_SPI_CLEAR_EOTFLAG(&hspi1);
__HAL_SPI_CLEAR_FREFLAG(&hspi1); //end SPISetup
}
}
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);
}
void spiISRSTM(SPI_HandleTypeDef *hspi) {
if (hspi->Instance->SR & SPI_FLAG_TXP) {
HAL_GPIO_WritePin(nFPINT_GPIO_Port, nFPINT_Pin, GPIO_PIN_RESET);//Lower nFPINT
(*(__IO uint8_t *)&hspi->Instance->TXDR) = 5; // transmit
__HAL_SPI_DISABLE_IT(hspi, SPI_IT_TXP); // disable TXP
while(!__HAL_SPI_GET_FLAG(hspi, SPI_FLAG_TXC)){}
byteXd = 1;
}
//Receive if ready
if (hspi->Instance->SR & SPI_FLAG_RXP) {
rxBuffer = (*(__IO uint8_t *)&hspi->Instance->RXDR);
byteRd = 1;
__HAL_SPI_DISABLE_IT(hspi, SPI_IT_RXP);
}
pPacketSlave->ProcessSPI(); //Process SPI data
HAL_GPIO_WritePin(nFPINT_GPIO_Port, nFPINT_Pin, GPIO_PIN_SET); //Raise nFPINT
__HAL_SPI_CLEAR_OVRFLAG(hspi);
__HAL_SPI_CLEAR_EOTFLAG(hspi);
__HAL_SPI_CLEAR_FREFLAG(hspi);
}
Master SPI:
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_MASTER;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 0x0;
hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
hspi2.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi2.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi2.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi2.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi2.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi2.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi2.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi2.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_ENABLE;
hspi2.Init.IOSwap = SPI_IO_SWAP_DISABLE;
if (HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
[ISRs]
void spiISRSTM(SPI_HandleTypeDef *hspi) {
if (hspi->Instance->SR & SPI_FLAG_TXP) {
SET_BIT(hspi->Instance->CR1, SPI_CR1_CSTART); // start SPI master
HAL_GPIO_WritePin(GPIOI, GPIO_PIN_0, GPIO_PIN_RESET); // Pull CS low
(*(__IO uint8_t *)&hspi->Instance->TXDR) = txBuffer; // transmit
__HAL_SPI_DISABLE_IT(hspi, SPI_IT_TXP); // disable TXP
while(!__HAL_SPI_GET_FLAG(hspi, SPI_FLAG_TXC)){}
HAL_GPIO_WritePin(GPIOI, GPIO_PIN_0, GPIO_PIN_SET); // Pull CS high
byteXd = 1;
}
//Receive if ready
if (hspi->Instance->SR & SPI_FLAG_RXP) {
rxBuffer = (*(__IO uint8_t *)&hspi->Instance->RXDR);
byteRd = 1;
__HAL_SPI_DISABLE_IT(hspi, SPI_IT_RXP);
}
__HAL_SPI_CLEAR_OVRFLAG(hspi);
__HAL_SPI_CLEAR_EOTFLAG(hspi);
__HAL_SPI_CLEAR_FREFLAG(hspi);
}
Solved! Go to Solution.
2024-11-19 1:15 AM
Hello @EthanMankins
You are not disabling the SPI peripheral at the end of transfer.
In the HAL SPI driver, the transfer is closed after checking the EOT flag.
/* Wait for Tx (and CRC) data to be sent */
if (SPI_WaitOnFlagUntilTimeout(hspi, SPI_FLAG_EOT, RESET, Timeout, tickstart) != HAL_OK)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_FLAG);
}
/* Call standard close procedure with error check */
SPI_CloseTransfer(hspi);
You can refer to the SPI_CloseTransfer() function below to implement the close procedure in your application.
static void SPI_CloseTransfer(SPI_HandleTypeDef *hspi)
{
uint32_t itflag = hspi->Instance->SR;
__HAL_SPI_CLEAR_EOTFLAG(hspi);
__HAL_SPI_CLEAR_TXTFFLAG(hspi);
/* Disable SPI peripheral */
__HAL_SPI_DISABLE(hspi);
/* Disable ITs */
__HAL_SPI_DISABLE_IT(hspi, (SPI_IT_EOT | SPI_IT_TXP | SPI_IT_RXP | SPI_IT_DXP | SPI_IT_UDR | SPI_IT_OVR | \
SPI_IT_FRE | SPI_IT_MODF));
/* Disable Tx DMA Request */
CLEAR_BIT(hspi->Instance->CFG1, SPI_CFG1_TXDMAEN | SPI_CFG1_RXDMAEN);
/* Report UnderRun error for non RX Only communication */
if (hspi->State != HAL_SPI_STATE_BUSY_RX)
{
if ((itflag & SPI_FLAG_UDR) != 0UL)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_UDR);
__HAL_SPI_CLEAR_UDRFLAG(hspi);
}
}
/* Report OverRun error for non TX Only communication */
if (hspi->State != HAL_SPI_STATE_BUSY_TX)
{
if ((itflag & SPI_FLAG_OVR) != 0UL)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_OVR);
__HAL_SPI_CLEAR_OVRFLAG(hspi);
}
#if (USE_SPI_CRC != 0UL)
/* Check if CRC error occurred */
if (hspi->Init.CRCCalculation == SPI_CRCCALCULATION_ENABLE)
{
if ((itflag & SPI_FLAG_CRCERR) != 0UL)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_CRC);
__HAL_SPI_CLEAR_CRCERRFLAG(hspi);
}
}
#endif /* USE_SPI_CRC */
}
/* SPI Mode Fault error interrupt occurred -------------------------------*/
if ((itflag & SPI_FLAG_MODF) != 0UL)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_MODF);
__HAL_SPI_CLEAR_MODFFLAG(hspi);
}
/* SPI Frame error interrupt occurred ------------------------------------*/
if ((itflag & SPI_FLAG_FRE) != 0UL)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_FRE);
__HAL_SPI_CLEAR_FREFLAG(hspi);
}
hspi->TxXferCount = (uint16_t)0UL;
hspi->RxXferCount = (uint16_t)0UL;
}
2024-11-19 1:15 AM
Hello @EthanMankins
You are not disabling the SPI peripheral at the end of transfer.
In the HAL SPI driver, the transfer is closed after checking the EOT flag.
/* Wait for Tx (and CRC) data to be sent */
if (SPI_WaitOnFlagUntilTimeout(hspi, SPI_FLAG_EOT, RESET, Timeout, tickstart) != HAL_OK)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_FLAG);
}
/* Call standard close procedure with error check */
SPI_CloseTransfer(hspi);
You can refer to the SPI_CloseTransfer() function below to implement the close procedure in your application.
static void SPI_CloseTransfer(SPI_HandleTypeDef *hspi)
{
uint32_t itflag = hspi->Instance->SR;
__HAL_SPI_CLEAR_EOTFLAG(hspi);
__HAL_SPI_CLEAR_TXTFFLAG(hspi);
/* Disable SPI peripheral */
__HAL_SPI_DISABLE(hspi);
/* Disable ITs */
__HAL_SPI_DISABLE_IT(hspi, (SPI_IT_EOT | SPI_IT_TXP | SPI_IT_RXP | SPI_IT_DXP | SPI_IT_UDR | SPI_IT_OVR | \
SPI_IT_FRE | SPI_IT_MODF));
/* Disable Tx DMA Request */
CLEAR_BIT(hspi->Instance->CFG1, SPI_CFG1_TXDMAEN | SPI_CFG1_RXDMAEN);
/* Report UnderRun error for non RX Only communication */
if (hspi->State != HAL_SPI_STATE_BUSY_RX)
{
if ((itflag & SPI_FLAG_UDR) != 0UL)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_UDR);
__HAL_SPI_CLEAR_UDRFLAG(hspi);
}
}
/* Report OverRun error for non TX Only communication */
if (hspi->State != HAL_SPI_STATE_BUSY_TX)
{
if ((itflag & SPI_FLAG_OVR) != 0UL)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_OVR);
__HAL_SPI_CLEAR_OVRFLAG(hspi);
}
#if (USE_SPI_CRC != 0UL)
/* Check if CRC error occurred */
if (hspi->Init.CRCCalculation == SPI_CRCCALCULATION_ENABLE)
{
if ((itflag & SPI_FLAG_CRCERR) != 0UL)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_CRC);
__HAL_SPI_CLEAR_CRCERRFLAG(hspi);
}
}
#endif /* USE_SPI_CRC */
}
/* SPI Mode Fault error interrupt occurred -------------------------------*/
if ((itflag & SPI_FLAG_MODF) != 0UL)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_MODF);
__HAL_SPI_CLEAR_MODFFLAG(hspi);
}
/* SPI Frame error interrupt occurred ------------------------------------*/
if ((itflag & SPI_FLAG_FRE) != 0UL)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_FRE);
__HAL_SPI_CLEAR_FREFLAG(hspi);
}
hspi->TxXferCount = (uint16_t)0UL;
hspi->RxXferCount = (uint16_t)0UL;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.