2024-02-14 2:16 AM
Hello,
I have problem with ping request and RNDIS server. I use STM32F746G-Discovery and Windows 7,10,11.
My steps:
- Deactivate IPv6 and activate IPv4 mode
- Static addresses as follows:
- Address = 192.168.0.11
- Network Mask = 255.255.255.0
- Gateway = 192.168.0.1
- Automatic DNS and Routing deactivated.
To restore communication I need to change the network settings. I have to set IP6 active and click OK.
Why is communication restored after IP6 activation? I think than communication should start after connect USB to PC. Can you explain to me what is the problem ?
Solved! Go to Solution.
2024-04-18 11:19 PM
Hi,
I believe the problem was the antivirus program. When I tested the device without an antivirus program it worked fine. Using Wireshark I could see that not all network packets were arriving.
I gave up using RNDIS over USB.
2024-03-01 6:32 AM
Hello @pferd
You are trying to run STM32746G-DISCOVERY_USBD-FS example from cube firmware without any modifications using our reference board MB1191-C03? You followed readme with no success?
If not, please don't hesitate to share your hardware setup and the minimum software to reproduce the issue.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-06 4:46 AM
Hello,
I used the example without any modifications:
...\STM32Cube_FW_F7_V1.17.1\Projects\STM32746G-Discovery\Applications\USB_Device\CDC_RNDIS_Server
I read "readme.txt" file.
I used your reference board MB1191 B-04 2155003701.
2024-03-12 4:45 AM
Hi @pferd
After several tests, I couldn't reproduce. It appears that deactivating and then reactivating IPV6 allows the target and the host to restore communication without any issues.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-18 11:19 PM
Hi,
I believe the problem was the antivirus program. When I tested the device without an antivirus program it worked fine. Using Wireshark I could see that not all network packets were arriving.
I gave up using RNDIS over USB.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.