2025-03-03 12:40 AM
We have a problem converting our running USB VCP application (RTOS) to a working RNDIS version.
if (USBD_RegisterClass(&hUsbDeviceHS, &USBD_CDC_RNDIS) != USBD_OK) {
while (1) {
}
}
hUsbDeviceHS.pClassData = USBD_malloc(sizeof(USBD_CDC_RNDIS_HandleTypeDef));
if (USBD_CDC_RNDIS_RegisterInterface(&hUsbDeviceHS, &USBD_CDC_RNDIS_fops) != USBD_OK)
{
while (1) {
}
}
The USB transfer is working for 1-2 seconds, but at the end the code stucks with an ISR queue overflow error.
Did anyone ever hear about such a problem? Or what do we miss in our initialization?
2025-04-24 8:16 AM
Hi @TKlem.1
We have a ready to use example using USBX. Otherwise, check the example provided for F7 used as CDC RNDIS server which may need some porting to fit H735 disco board.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.