STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeIDE not showing stm32c0 series - when starting new project (screenshot attached).

 When I am trying to create a new project for STM32C011 series microcontroller, STM32 cube IDE not showing it in microcontroller selection list.Do i need to install support/package for STM32C0 series, to create workspace for the STM32C0 workspace.Tha...

DalipSharma_0-1699291907180.png

Resolved! STM32L4 DMA setup

I have a question about DMA in the STM32L432 (and presumably similar more most STM32L4* devices). The background is that I'm trying to set up timer #2 driving a DAC, and have the DAC grab new data from a circular buffer via DMA.In the RM0394 referenc...

joelG by Associate
  • 3128 Views
  • 2 replies
  • 0 kudos

Nucleo-C031C6 ADC maximum clock speed

Hello,I have an issue with the maximum speed of the ADC clock for Nucleo-C031C6. In the device datasheet, it states that the max clock speed is 35 MHz. However, in STM32 CubeIDE, I have the option to select the asynchronous clock mode, and DIV1 is ac...

DDjur.1 by Associate II
  • 2172 Views
  • 3 replies
  • 1 kudos

UCPD DRP DCDC power management through I2C

Hello,I am implementing a DRP device that is to be connected to a battery.I have this DRP example setup with the X-NUCLEO-DRP1M1 and a NUCLEO-G071RB. It is working with a 5V profile and a fixed 5V supply.I have added a 9V source PDO in CubeMX, and ca...

NMartin_0-1698799399113.png
NMartin by Associate III
  • 1915 Views
  • 1 replies
  • 0 kudos

Getting data from SAI interface (microphone array)

Hi. I want to make microphone array with 16 ICS-52000 microphones connected to STM32L476RG. I made 16 PCB's and now I want to test each microphone and display some data in console just to see if they just work properly. Below is my SAI config: ICS-5...

erysv_0-1698606561673.png
erysv by Associate II
  • 2542 Views
  • 2 replies
  • 0 kudos

Bug STM32F429ZI ETH PTP TIM2 ITR1

STM32Cube FW_F4 V1.27.1HAL ETH PTPfilestm32f4xx_hal_tim_ex.cDefinition of TIM_TIM2_ETH_PTPline 75-79#if defined(TIM8)#define TIM_TIM2_TIM8_TRGO           0x00000000U               /*!< TIM2 ITR1 is connected to TIM8 TRGO */#else#define TIM_TIM2_ETH_P...

vekli by Associate II
  • 2918 Views
  • 4 replies
  • 2 kudos

STM32f407 dma->uart transfer stops after some time

Hi, i have a certain problem.I have an application which continuously reads out data from sensors. Each sensor read will be triggered by me by using a dma-uart transaction. On the receiving side i have a uart-dma in cyclic mode which fills up the buf...

MOtto.1 by Associate II
  • 9360 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.